STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

UART1 RAK3172 (STM32WLE5CCU6)

  Hello, I’m facing an issue using the RAK3172. In my project, UART1 is configured for debugging and LoRaWAN logs, while UART1 (PB6/PB7) is reserved for communication with the LC76G GPS module. However, I'm unable to print any data from the GPS modul...

samuelbs by Associate III
  • 2797 Views
  • 11 replies
  • 1 kudos

Resolved! STM32 MCU model shortlisting for Making RC remote

Hi everyone,which type of stm32 microcontroller is best fit for following operationsfor building rc remote of 8 channel and morelow costlow power consumptionhigh-speed rf communication and easy integrate with RF chip using SPI porteasy to design and ...

Palnerve by Associate
  • 696 Views
  • 2 replies
  • 0 kudos

Resolved! STM32WB55RG, Warning: FUS_STATE_IMG_NOT_FOUND

Hello,I am working on the NUCLEO-WB55RG. I have updated the FUS to v2.1.0.0 and then loaded the stm32wb5x_BLE_Stack_full_fw v1.23.0. This worked fine.After that, I wanted to load the stm32wb5x_BLE_Stack_full_extended_fw.bin, but now I always get the ...

Stabilo_0-1751901998880.png Stabilo_1-1751902064593.png
Stabilo by Associate III
  • 660 Views
  • 1 replies
  • 0 kudos

Resolved! No `pin reservation` and GPIO initialization as a resutl

HelloI have the issue, GPIO pin initialization to specified mode isn`t generated.I can`t find ''pin reservation'' in pop-up from right click on pin or in any tab (pinout & configuration -> gpio mode configuration)It`s dual-core project for stm32wl55j...

nuksirp by Associate
  • 517 Views
  • 1 replies
  • 0 kudos

Resolved! STM32WL33 RF868MHz LC circuit matching

We are developing SIgfox with STM32WL33KBV6, and we don't know how to deal with the 826-958MHz RF partial matching circuit, so we hope you can help.There is no specific reference value for this part of the circuit for the LC component.  

KiteLee_0-1751507071537.png
KiteLee by Associate II
  • 891 Views
  • 1 replies
  • 0 kudos

Resolved! X-NUCLEO-WB05KN1 with NUCLEO-U545RE-Q

I would like to make a basic application using BLE (to turn on an LED). I’m using the WB05KN1 shield and my application runs on the U545. I would like to know if it’s possible to carry out this project, if they are compatible, and if you know where I...

Resolved! STM32WL - SUBGHZSPI DEBUG

For a project of mine, I wanted a LoRa Transceiver like (like the SX1262) to be controlled by a host application running on a STM32F4. I have a few STM32WLE5CCU6s lying around from a previous project, and was thinking if I could use them instead. The...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.