cancel
Showing results for 
Search instead for 
Did you mean: 

X-NUCLEO-WB05KN1 with NUCLEO-U545RE-Q

sheulisback
Associate II

I would like to make a basic application using BLE (to turn on an LED). I’m using the WB05KN1 shield and my application runs on the U545. I would like to know if it’s possible to carry out this project, if they are compatible, and if you know where I can find example codes because I can only find examples with Zephyr.ephyr.

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @sheulisback and welcome to the ST Community.

The X-NUCLEO-WB05KN1 can be plugged into an STM32 Nucleo development board (such as the NUCLEO-U545RE-Q that you are using). For the examples, you can inspire from those on the X-CUBE-WB05N that are made to be compatible with the NUCLEO-U575ZI-Q. There is no example based on the NUCLEO-U545RE-Q.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
STTwo-32
ST Employee

Hello @sheulisback and welcome to the ST Community.

The X-NUCLEO-WB05KN1 can be plugged into an STM32 Nucleo development board (such as the NUCLEO-U545RE-Q that you are using). For the examples, you can inspire from those on the X-CUBE-WB05N that are made to be compatible with the NUCLEO-U575ZI-Q. There is no example based on the NUCLEO-U545RE-Q.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

sheulisback
Associate II

Thank you for your reply.
If I manage to complete a project, I will post it on GitHub and share the link here

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.