2018-01-10 10:54 PM
I have a Murata LoRa SOC from which I have made up a custom board and I am flashing code using UART which wasn't successful until help from
https://community.st.com/people/Turvey.Clive.002
Now I am using stm32flash open source software for flashing of code but after successful flashing I still am not even able to blink a LED using the flashed code. While the software did work when flashed to DISCOVERY kit.
I reckon this must be because the ICs aren't shipped with bootloader? Is it? But then how did the flashing work? I am so confused. Please help.
PS: Boot configurations are perfectly alright.
#stm32l0 #b-l072z-lrwan1 Note: this post was migrated and contained many threaded conversations, some content may be missing.2018-01-11 12:08 AM
Are your custom board and the Discovery using the same MCU type ?
Are the LEDs you try to blink on the same pin(s) ?
Are the clock source (quartz, frequency) the same ?
I reckon this must be because the ICs aren't shipped with bootloader?
If you mean the system bootloader (entered via BOOT0/BOOT1), no.
This bootloader is in ROM, and always present.
I don't know any Discovery kit that uses a second-stage bootloader.
But if your LoRa SoC has such a second stage BL, it most probably conflichts with your test application.
I would try a JTAG/SWD adaptor (like STLink) to flash, and a toolchain.
2018-01-11 1:36 AM
SARTHAK KELAPURE wrote:
I have a Murata LoRa SOC
You mean the 'Type ABZ' module:
https://wireless.murata.com/eng/products/rf-modules-1/lpwa/type-abz.html
Note that this is not a SoC; it is an
STM32L072 microcontroller and a Semtech SX1276 Radio - two separate chips.
Sorry - I can't see the rest of your text due to the forum faults.
2018-01-11 7:47 AM
In another post you indicate the lack of SWD (SWCLK,SWDIO), hopefully you have at least test points or edge castellations where you can access these signals, otherwise your design is going to be a bit of a bear to debug and bring up.
The BOOT0 high configuration seems to get you into the loader. In normal operation this should be pulled low. You should also be able to read out the code written to confirm the correct delivery.
You will need to simplify your test code so you can see how far beyond Reset_Handler you get. You should perhaps just let the part run of the initial clock rather than change them or enable the PLL.
I might start by adding code into the Reset_Handler to enable a GPIO clock, and a GPIO pin, and then toggle that in a way I can scope to prove the part is alive, and that my code can run. Once you have done that look for code that sticks in spin loops or bombs silently into Error_Handler(), etc.
2018-01-11 8:50 AM
The user activity tab should provide 'Show More' to expand most things. Attachments seem to be an issue, perhaps the cause of the error. Jive's rapid response team of agile programmers is hard at work....
2018-01-11 9:19 AM
It won't expand the OP - just the following 'activity'
:(
2018-01-11 9:57 AM
can see the whole thing in 'inbox' view.
2018-01-11 10:07 AM
I was just waiting for your reply and with a new update on my situation I am sure you will be able to help,
I am now able to flash using the STM32Cube Programmer. While flashing I kept the BOOT0 low and flashed using UART to address 0x08008000 and without a restart I get the expected output of blinking LEDs. But on restart/reset of my board the application stops working. While the STM32Cube Programmer shows the hex values of all pages, I tried match all the values(from blink.bin and 0x08008000 onwards) and they were same.
What may be the issue and how do we solve?
2018-01-11 10:18 AM
The processor pulls initial PC and SP from a Vector Table that it expects to be at 0x08000000. Not sure how it would get to 0x08008000 without some loader code earlier in FLASH to transfer control there.
2018-01-11 10:21 AM
Well correct, I tried 0x08000000 also but the reset thing still persists.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.