STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4119 Views
  • 0 replies
  • 3 kudos

Resolved! Trying to build the end node node application for B-L072Z-LRWAN1 from STM32CubeExpansion_LRWAN_V1.2.1 in keil ide [MDK-ARM Version 5.28a ] but it gives a code size error:

error:.\mlm32l07x01\NUCLEO_CUBE_LORA.axf: error: L6050U: The code size of this image (52352 bytes) exceeds the maximum allowed for this version of the linker.Finished: 0 information, 0 warning, 0 error and 1 fatal error messages.".\mlm32l07x01\NUCLEO...

Msing.4 by Associate II
  • 1646 Views
  • 1 replies
  • 0 kudos

ATT_MTU size

HI,Does someone can explain me how to modify the ATT MTU size please ?Thanks.

LVent by Associate II
  • 3944 Views
  • 5 replies
  • 0 kudos

How to create a private service in the firmware?

There is a heart rate service example in the STM32WB firmware. If I want to create a private service in the firmware. For example​, I want to create a service to let the LED on and OFF. How to create a private service like that?

Rzou by Associate
  • 646 Views
  • 0 replies
  • 0 kudos

Resolved! Modify Ping-Pong example

Hi guys,I program an application with a STM32LO-LRWAN1 module who does the connection with a sensor by I2C and i would like to integer my application in the "Ping Pong" example for proving to my boss that the connection between two modules is possibl...

mibou23 by Associate II
  • 3002 Views
  • 4 replies
  • 0 kudos

Resolved! Iam unable to debug STM32 B-L0722Z-LRWAN1 board having onboard STM32L072CZ MCU. It gets programmed but no respose for breakpoints and also unable to suspend

Attaching the log files.Open On-Chip Debugger 0.10.0+dev-00021-g524e8c8 (2019-04-23-20:37)Licensed under GNU GPL v2For bug reports, read http://openocd.org/doc/doxygen/bugs.htmlsrst_only separate srst_nogate srst_open_drain connect_assert_srstInfo : ...

Resolved! where can I download the AN5289

I want to build the wireless application. I see the an5289 is a guide for that. but I can't find where I can download it.

cchao by Associate II
  • 1939 Views
  • 5 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.