2019-06-19 11:40 PM
HI,
Does someone can explain me how to modify the ATT MTU size please ?
Thanks.
2019-06-20 1:00 AM
Hi, Leo.
Do not wait for a response from the STM employees, they do not answer questions about the WB55.
I have analyzed and found out:
There is only one place where you can set the MTU, it is in a calling function SHCI_C2_BLE_Init(&ble_init_cmd_packet);
where in structure SHCI_C2_Ble_Init_Cmd_Packet_t ble_init_cmd_packet
we set CFG_BLE_MAX_ATT_MTU (#define CFG_BLE_MAX_ATT_MTU (512)).
As it is not surprising, but STM no longer has any opportunity to change the MTU.
There is one function (aci_gatt_exchange_config) but, unfortunately, for some reason it does not allow to set a different value for MTU (this is a question for the STM, but it’s useless to ask questions, you can look in my profile how much I asked about this chip).
On the other hand, it is not recommended to call aci_gatt_exchange_config if we are peripherals, so I addressed this question like this:
I set MTU, for example, = 512.
The apple itself requests the MTU after the connection, so in the EVT_BLUE_ATT_EXCHANGE_MTU_RESP event, we catch the MTU of the apple and get what we are walking.
The Android itself does not send such a request, therefore, if in the android application you need to force the function gatt.requestMtu (***), in this case, receive the event EVT_BLUE_ATT_EXCHANGE_MTU_RESP.
According to my experience:
iPhone6s - MTU=185
Android - defult =23, but if you call gatt.requestMtu on android side, get what you want.
iPhone8 - MTU = 527.
Regards,
Vyacheslav.
2019-06-20 1:34 AM
It is possible to modify CFG_BLE_MAX_ATT_MTU in the app_conf.h file.
This means that it can be done during the init phase using the SHCI_C2_Ble_Init_Cmd_Packet_t ble_init_cmd_packet structure.
it can also be dynamically done after the connection is established with a GATT message: aci_gatt_exchange_config.
An ACI_ATT_EXCHANGE_MTU_RESP_EVENT event is generated from which the MAX_ATT_MTU value can be extracted.
Then this value can be used to set the new packet size.
Please have a look at the AN5289 application note "Building wireless applications with STM32WB Series microcontrollers" that is now available on the st.com web site.
There are some explanations on this topic: 7.6.5 How to maximize data throughput
2019-06-20 1:44 AM
Thanks.
It doesn't work when I change the MTU size in app_conf.h in both sides
I suppose that I need to modify CFG_BLE_PREPARE_WRITE_LIST_SIZE too ?
I tried to modify CFG_BLE_PREPARE_WRITE_LIST_SIZE which is defined by default to 0x3A, why this value ?
When I’m doing my own calculous for the packet size with ATT_MTU =23 bytes I find 0x25.
So please, tell me how to change the MTU size correctly.
Regards,
Léo.
2019-06-24 7:37 AM
What is your wished value for ATT_MTU ? Did you send the aci_gatt_exchange_config command?
2019-06-24 8:20 AM
Between 23 and 512 bytes.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.