STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

ping pong with lora doesn't recieve anything working on theboard B-l072Z-LRWAN1 with I-CUBE-LRWAN firmware packag?

I'm working with the ping pong with lora in stm32 , the code doesn't recieve anything , it only executes the RX_timeout and TX_timeout while the device in the other side is sending DATA correctly with lora, How can I fix this problem ?this is in the ...

AChaa.15 by Associate II
  • 1032 Views
  • 1 replies
  • 0 kudos

STM32 LRWAN-1

Hi guys,I try to establish connection between two STM32L072CZY6TR with the programme ping pong include in the I-CUBE LRWAN1 Package.The goal is that one board work with the external battery and that the other board is connected with the computer.I re...

mibou23 by Associate II
  • 790 Views
  • 0 replies
  • 0 kudos

Resolved! I-CUBE-LRWAN ping pong example

Hi all,I am modifing the Ping Pong example of the I-CUBE-LRWAN; I am working with a L073RZ nucleo board and the SX1272MB2xAS LoRa shield.I was performing some experiment (changing spreading factor, code rate, bandwidth) and the example with SF = 11 a...

clf88 by Associate
  • 2339 Views
  • 3 replies
  • 0 kudos

Resolved! Where can I get STM32WBxx_SW_Architecture_and_Design.pdf ?

I read mac_802_15_4_api_wb.c and Inside it mentioned "Check STM32WBxx_SW_Architecture_and_Design.pdf for further information".I searched this file, but I could not get it.So,where can I get STM32WBxx_SW_Architecture_and_Design.pdf ?

STana by Associate
  • 1339 Views
  • 2 replies
  • 0 kudos

Cannot reprogram B-L072Z LoRaWAN Discovery board.

I have a B-L072Z LoRa dev board that I am unable to reprogram. ST-Link drivers are installed and the device communicates to my PC terminal via the virtual COM port without issue. When I attempt to flash the board with a new binary, it appears to repr...

ty.locke by Associate II
  • 2128 Views
  • 4 replies
  • 0 kudos

Characteristic with write and notification parameter: the data automatically sent back to the device after write to.

STM32WB55Why I can`t post question in any group?This question i want to post in STM32WB55 but receive error "You can't add new topics, so select existing topics for your post"Hi.I use characteristic with properties: CHAR_PROP_WRITE | CHAR_PROP_NOTIFY...

Ada controlling the STM32WB

I ported AdaCore's opensource Ada toolchain to the STM32WB. I made a workalike of the dongles client demo. So far, so good!http://www.hrrzi.com/2019/06/ada-on-stm32wb.htmlHave fun!

Hedley by Associate III
  • 967 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.