NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I am using STM32Cube FW_WB V1.1.1 and built a new project.I have programmed stm32wb5x_BLE_Stack_fw.bin into the memory space for CPU2 (0x80CB000).I have added the following interrupt handlers:void IPCC_C1_TX_IRQHandler(void) { HW_IPCC_Tx_Handler();...
Hi, does somebody knows, is STM32WB55 support LE Codded or LE 1M or LE 2M?Does this MCU supports Long range connectivity?--best regards,Sergii
Dear all,The following are codes of SAI protocol and dma init.The MCU I using was stm32wb. Then i use HAL_SAI_Receive_DMA(); to receive the microphone senor data in standard i2s protocol,but i the receive data is 0.Did i need to modify in DMA set...
Hi All; Previously, I use to firmware version 1.2.1 is working with LoRa server version 1.0.2 according LoRa alliance. Now I use to firmware version 1.2.2 is not working. I can send data in OTAA mode. I see Join Request and Join Accept but I can't s...
Hi,I am using B-L072Z-LRWAN1and AT-Slave project from I-Cube-LORAWAN SDK. What sequence of AT commands should the host issue to Join the network in OTAA mode and send data. Currently, I am using AT+JOIN and AT+SEND. But with these commands, I am not ...
I'm using the P-NUCLEO-WB55 development board, and I'm using the IDE to auto-generate the project/code.However, the default linker script is mis-configured.indeed, the _estack variable is set to 0x2003FFFF instead of 0x20030000.The first address is w...
Hello to everyone, I don't have a gateway but two B-L072Z-LRWAN1 kits. So I am trying to send a sensor data between these kits. ST has i-cube-lrwan library for kit but it is not compatible with CubeMX and very complex because of LoRaWAN. I have used ...
Hi, I am developing software based on the l-CUBE LRWAN software and ran into some low power issues. I have a sensor connected to the USART2 and it is receiving data properly. The problem is that because i had to overwrite the void HAL_UART_MspInit(U...
Hello,I'm a beginner with STM32CubeIDE environment and I'm having a lot of troubles trying to run Application examples download from the STM32Cube MCU Packages.What is the right way to import projects. As an example I'm trying to import the BLE_p2pSe...
Hello, I bought the P-Nucleo-WB55 kit but I'm having problems running the examples provided.I have overwritten by mistake the demo firmware available in the P-Nucleo-68 and now I would like to download back the demo firmware again starting from the d...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.