2019-05-21 3:43 AM
Hi,
I am developing software based on the l-CUBE LRWAN software and ran into some low power issues. I have a sensor connected to the USART2 and it is receiving data properly. The problem is that because i had to overwrite the void HAL_UART_MspInit(UART_HandleTypeDef *huart) (located in vcom.c) function the device doesnt get into the lowpower mode.
When the sensor is working the current consumption in lowpowermode is around 4.0mA
When I dont overwrite the fuction (And thus dont have a working sensor) the current in LPM is around 4uA.
2019-07-11 4:04 AM
hiii bro
i know you are asking, but i think you can help me in my problem:
I use the node B-L072Z-LRWAN1 with the example “end node�? of the stack “STM32CubeExpansion_LRWAN�?, the objectif it’s to send data of sensor to TTN. and I managed to send “int�? or "floa"t without problem to my TTN as first step.
on the other hand, I made a program of UART communication of the “B-L072Z-LRWAN1�? thanks to STM32CubeMX, and it’s working well.
Unfortunately I don’t know how integrated all the code that STM32CubeMX generated in the “end node�? project to send my UART data.
thanks in advence.
2019-07-11 5:42 AM
2019-07-12 1:21 AM
i see, in my case i have a sensor connected to the USART2 too, when i make a code using cubemx it's working but when i try to integrate it with the end node exemple it give nothing.
please if you can help me with that it's urgent.
2019-07-18 12:31 AM
Hi,
Do you have the same problem when you connect the sensor to usart1?
2019-07-18 2:54 AM
thank you so much for your replay, i apreciate it
i tried the USART2 it gaves the same result, please if you can help me with that problem because I'm stuck .
2019-07-29 12:44 AM
The USART2 is allready initialized in the vcom filles for the usb communication. You could try to remove all these functions and init your sensor. This solved the problems i had with USART2.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.