NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hlw Sir,I am piyush kumar having a STM32F030 Nucleo Board and one ESP8266 WIFI Module.I am very new to IOT . Can you please guide me on this how can i start IOT with these two.
Hi,Does somebody have any application notes or some articles, that describes, how to run BLE example under STM32CubeIDE and debug it there?--Best regards,Sergii
Hello, i have two b-l072z board and making LoRa comm as point to point. While I sending ADC data I want to add packet to timestamp. I have inspected hw_rtc.c file and find HW_RTC_GetCalenderValue function. But it make me confusing because of static...
I am having problems running LPTIM1 off the LSE. When I set up and interrupt it is firing ever clock cycle and does not seem to be clearing. RCC_BDCR_LSERDY bit is active before selecting the LPTIM1 clock source. I have also tried disabling the inter...
I read that STM32WB current models do not currently support a Bluetooth 5 coded PHY. Is it possible it will someday with an upgrade to the CoProc Binaries, or is it not in the silicon at all?If not does ST have any parts on the roadmap that will?
Hi, I am new programming with STM microcontrollers and I would need to to program the B-L072Z-LRWAN1 development board with the Adafruit Ultimate GPS module quickly. The idea is to see the GPS data in the simplest way.Could you please help with this?...
I'm using BLE_p2pRouteur example code. In app_conf.h, CFG_TX_POWER is #defined to 0x18, and the comment next to it says 0 dbm. This parameter gets passed to aci_hal_set_tx_power_level(1, CFG_TX_POWER). The documentation of this function in UM1865 ...
Hi guys,im working on project with STM32WB55RG and noticed very strange behaviour of RTC peripheral.After power up everything works fine but after reset RTC peripheral won't initialize. I'm using HAL library. After further investigation of code I've ...
I have been looking into ways to implement Thread network co-processor (NCP) with STM32WB and could no find any.
Hello,From where I can get the HDP profile example of STM32 MCUs?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.