NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I have WB55 Dongle board that someone may have programmed previously. I am trying to start it fresh and make sure it is up to date using all files from from STM32Cube_FW_WB_V1.2.0I followed the procedure to install new FUS and BLE Stack:STM32_Progr...
The STM32WB55xx devices embed an Arm ®(a) CPU1 Cortex ® -M4 core.I use this chip manual.I operate strictly according to the chip manual, but all of them have errors in reading, writing and erasing a sector.the flash meomory address range:0x0800 000-...
Hi Sir/Madam,Here i need calculate the current required to operate the STM32WB55REvx. I downloaded the datasheet of this MCU. In the datasheet should i need to consider the operating conditions or absolute characteristics to calculate the current re...
FLASH address: 0x0800 0000~0x080F 5FFF, CPU1 (cortex-M4) can read and write to its normal access, address 0x080F 6000~0x080F FFFF is protected by CPU2 (cortex-M0)and read and write.
Hi,I am a new to STM32WB55 Nucleo and have just started to understand it from the examples provided by the ST. In this process, I have observed unknown data format on hyper terminal. i tried with different baudrates and all the available UART library...
Using STM32Cube, I can build the demo project MOTENV1_IKS01A3_WB55RG fresh from the zipfile fine. However, you cannot open the MOTENV1_IKS01A3_WB55RG.ioc file in it's original location. You get and error that it is the wrong name. So I copy MOTENV1_I...
Specifically, I am trying to compile the STM32WB Dongle Thread General CoAP example. Although this isn't a problem specific to STM32 but more with the IDE, I was hoping somebody might have a hint on how to solve the issue. Also, all of the files exis...
Hello,I'm currently developing an application on the STM32WB55 that utilises IEEE802.15.4 communication. Based on the example application project from the STM32Cube_FW_WB_V1.2.0 package (802.15.4 MAC), I was able to successfully (well, at least to so...
Hi,I'm using STM32WB55 controller in my project for low power BLE. But I have zero knowledge on BLE. Can any one help me in understanding from basics of BLE.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.