2019-11-15 12:40 PM
How change mbed linker for STM32WB55 to used STM_OTA bootloader (need to add TAG_OTA_START, TAG_OTA_END ...). This is my code but don't work, mbed given my error:
; #if !defined(MBED_APP_START)
; #define MBED_APP_START 0x08000000
#define MBED_APP_START 0x08007000
; #endif
; #if !defined(MBED_APP_SIZE)
; 768KB FLASH
; #define MBED_APP_SIZE 0xC0000
; 768KB FLASH - 0x7000 = 0xB9000
#define MBED_APP_SIZE 0xB9000
; #endif
#if !defined(MBED_BOOT_STACK_SIZE)
#define MBED_BOOT_STACK_SIZE 0x400
#endif
#define Stack_Size MBED_BOOT_STACK_SIZE
; 768KB FLASH (0xC0000) + 192KB SRAM (0x30000) + Shared mem
LR_IROM1 MBED_APP_START 0x184 { ; load region size_region
ER_IROM1_LOW MBED_APP_START 0x184 { ; load address = execution address
*.o (RESET, +First)
*.o(TAG_OTA_START)
}
; Total: 79 vectors = 316 bytes (0x13C) to be reserved in RAM
; RW_IRAM1 (0x20000000+0x13C) (0x30000-0x13C-Stack_Size) { ; RW data
RW_IRAM1 (0x20000004+0x13C) (0x30000-0x13C-Stack_Size-0x4) { ; RW data -< new value
.ANY (+RW +ZI)
}
ARM_LIB_STACK (0x20000000+0x30000) EMPTY -Stack_Size { ; stack
}
; SRAM2 - Shared memory
RW_IRAM2a 0x20030000 0x00002800 { ; RW data
*(MAPPING_TABLE)
*(MB_MEM1)
}
RW_IRAM2b 0x20038000 0x00005000 { ; RW data
*(MB_MEM2)
}
}
LR_IROM3 (MBED_APP_START + 0x184) (MBED_APP_SIZE - 0x184) {
ER_IROM1_HIGH (MBED_APP_START + 0x184) (MBED_APP_SIZE - 0x184) { ; load address = execution address
*(InRoot$$Sections)
.ANY (+RO)
*.o(TAG_OTA_END)
}
}error:
"BUILD/NUCLEO_WB55RG/ARMC6/.link_script.sct", line 61 (column 8): Warning: L6314W: No section matches pattern *.o(TAG_OTA_START).
"BUILD/NUCLEO_WB55RG/ARMC6/.link_script.sct", line 87 (column 9): Warning: L6314W: No section matches pattern *.o(TAG_OTA_END).
Error: L6220E: Load region LR_IROM1 size (488 bytes) exceeds limit (388 bytes). Region contains 75 bytes of padding and 0 bytes of veneers (total 75 bytes of linker generated content).
Error: L6221E: Load region LR_IROM1 with Load range [0x08007000,0x080071e8) overlaps with Load region LR_IROM3 with Load range [0x08007184,0x0802dc84).
Finished: 0 information, 13 warning and 2 error messages.When I rewrite linker I use uVision linker in "en.stm32cubewb\STM32Cube_FW_WB_V1.2.0\Projects\P-NUCLEO-WB55.Nucleo\Applications\BLE\BLE_HeartRate_ota" package with a few example but not to mbed :(
I written about this problem at mbed forum on github. I written there many details and describe what i did till now.
I don't wont duplicate all my posts - sorry for that, please go to the link https://github.com/ARMmbed/mbed-os/issues/11864
Thanks for help.
2019-11-15 2:36 PM
Hi,
Linker remove unused sections.
If you code contains (and it should contain it):
PLACE_IN_SECTION("TAG_OTA_END") const uint32_t MagicKeywordValue = 0x94448A29 ;
PLACE_IN_SECTION("TAG_OTA_START") const uint32_t MagicKeywordAddress = (uint32_t)&MagicKeywordValue;
but these variables are not used anywhere in the code, so the linker remove it out.
In order to remain them, you need to write a linker options
--keep *.o(TAG_OTA_START)
--keep *.o(TAG_OTA_END)
but I dont know where to do in Mbed studio .
About overlap error - look at the scatter file in SDK 1.3.0, maybe it will help you.
Regards,
Vyacheslav.
2019-11-19 6:43 AM
For example in the STM32Cube_FW_WB_V1.3.0\Projects\P-NUCLEO-WB55.Nucleo\Applications\BLE\BLE_HeartRate_ota directory, under the /STM32_WPAN\App you can find in the app_ble.c file the placement of these 2 values
PLACE_IN_SECTION("TAG_OTA_END") const uint32_t MagicKeywordValue = 0x94448A29 ;
PLACE_IN_SECTION("TAG_OTA_START") const uint32_t MagicKeywordAddress = (uint32_t)&MagicKeywordValue;
Have also a look in the scatter file .ld in the SW4STM32\BLE_HeartRate_ota directory where the 2 sections are logged in 2 different memory areas FALSH and OTA_TAG.
TAG_OTA_START : { KEEP (*(TAG_OTA_START)) } >FLASH
T AG_OTA_END : { KEEP (*(TAG_OTA_END)) } >OTA_TAG
These 2 MEMORY areas are defined at the beginning of this scatter file by
/* Specify the memory areas */
MEMORY
{
FLASH (rx) : ORIGIN = 0x08007000, LENGTH = 1k
RAM1 (xrw) : ORIGIN = 0x20000004, LENGTH = 191k
RAM_SHARED (xrw) : ORIGIN = 0x20030000, LENGTH = 10k
OTA_TAG (rx) : ORIGIN = 0x08007178 , LENGTH = 599k
}
You have to replicate this declaration scheme with mbed IDE.
2019-11-19 7:16 AM
Regarding the second error, The size of the data you located inside the LR_IROM1 section (488bytes = 0x1e8) is exceeding the reserved size (388 bytes = 0x184). Hence it overlaps with the next LR_IRPM3 section. Check the data size of the (Reset, + First) area.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.