NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi,I need help in develop ble mesh firmware for STM32WB. The main problem I have is connectivity. For tests I have two ble mesh nodes. Everything works fine when both nodes are powered on at the same time, the communication is from node1 to node2 and...
기존�?는 정해진 센서 �?��?�터를 보내기만 하여서, PC�?서 �?하는 입력�?� 쓰고 받고와 같�?� 가변�?�?� �?��?�터를 어떻게 전달하고 받아야하는지, 내부 버�?�를 어떻게 할당해주어야 하는지 잘 모르겠습니다. 참고할만한 예제나 코드를 어떤�?으로 구성해야하는지 알려주시면 �?사하겠습니다.기존�?� 무�?�타 모듈�?� Bin 파�?�과 AT Command Tool�?� 제공받아 중간 MCU 없�?� 따로 �?�작�?� 확...
I am working with a stm32 nucleo pack and I was using the end node code example. Our gateway is set up perfectly fine and running and we now have a working node that prints time outs on the CLI . How do we get the board to connect to the gate way? i...
Is it possible to jump from user program directly to USB DFU ?If affirmative, what is the address ?The idea is to allow USB firmware updates of a physically protected product without access to BOOT0 pin.
My project consists of two STM32WB A master and a slave. The master will run the p2pRrouter example with some modifications and the slave will run the p2pServer preferably with two connections.both Master and slave needs to communicate with each othe...
I stupidly used the mbed application and can no longer flash the WB55 Nucleo from Atollic or command line programmer.Have I flashed the STlink device instead of the WB55?How do I resurrect the Nucleo board.ThanksIan
I have a problem while using BLE using STM32WB55CG in my custom board.I tried steps explained on UM2550 - 5. How to flash the wireless coprocessor binary.But the custom board doesn't have any USB port so I tried to upload with ST-LINK(SWD).And I ...
I have a Raspberry Pi and an NCP running as the OpenThread Border Router. The thread commissioning Android app is used to add STM32WB nodes to the thread network. It requires the EUI64 for each device. If I read the eui64 via CLI, I can successfully ...
Hi,I am working with BLE_MeshLightingDemo. I have a problem with provisioning because device getting unprovisioned state after reset. It is strange because if I flash example BLE_MeshLIghtingDemo without modifying it everything works well. And next i...
I am trying to compile the BLE_DataThroughput example project. First, I started with CubeIDE. The program compiles for BLE central, but does not behave as expected on the hardware. For peripheral (#define CFG_BLE_CENTRAL 0) there are unknown symbols ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.