NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello, I want to use the last page of the flash memory.The last page of the STM32WB55CG is page 255 @ 0x080F F000 - 0x080F FFFF, 4 K, Page 255But, when I look at memory window, during run-time, I see there is nothing.See attached picwhere is the memo...
The reason for the question is to locate all errors and warnings into a single function so as not to have error handler fuctions located in several places in the code. does anyone have this request previously implemented and can give some input here....
I am looking for application notes with sample code to configure and setup Interrupt Service Routines using the NVIC of the CortexM4 in the STM32WB55.thanks
I am trying to use STM32CubeMonitor-RF to tune the HSE of a custom board but cannot find the script files needed to follow the example procedure outlined in the documentation (https://www.st.com/content/ccc/resource/technical/document/application_not...
I am issuing the following commands via USB:!deviceeui=323732385C377408!joineui=70B3D57ED002B102!appkey=DA7D3CC452FB6DEBEE88FBE8E40E0925!sysreset--Wait for reset --?devicejoinparamThe unit prints out the old info and never updates with the new keys. ...
I had purchased two STM32 Lora and Sigfox Discovery kit for STM32F072 MCU.I am using this for sigfox data transmitting purpose for our prototype designing . I had uploaded the AT commands code on both dev.boards, One board is completely working and t...
Hello,Is there GPIO support for antenna diversity on the STM32WL? The SX126x has dedicated gpio that can be configured to toggle automatically when in RX/TX mode. This is very important when in low duty cycle modes of operation because then the MCU...
STM32WB code for ble client in stm32cubeIDE gives error no configuration for device name , device address are available.
Dear sir,I using the Transparent Mode(BLE_TransparentModeVCP) to communicate with the STM32WB55 USB dongle.When I chick "connect" is show blow warning message. May I ask How to fix it?
I have a Nucleo pack. I loaded the Bluetooth test files (.HEX) into the main board and the dongle that comes in the pack and the code is working as explained. However when I compiled (Hex code not provided) and loaded ZigBee code, the unit is display...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.