2020-06-04 7:04 AM
Hi,
i have a system with 4 demoboard STM32WB55NUCLEO and 3 STM32WB55DONGLE. One nucleo is a P2P Client, the other 6 are P2P Server. I have modified the examples P2PClient and P2PServer for:
What happens: the connection manager that i created in the client connects and pair the servers one by one. The connection, pairing and communication work fine.
When I reboot a server, the client retreive an EVT_DISCONN_COMPLETE in which the state of the connection "i" is reset to APP_BLE_IDLE. When the connection manager relaunch the aci_gap_create_connection to reconnect the server, the return is the error 0x41, that is not in the standard return values of the function.
What is the mistake? Do i have to call some particular function in the EVT_DISCONN_COMPLETE for reset some status? What does mean that error code?
Thanks you in advance
Lorenzo
Solved! Go to Solution.
2020-06-11 12:06 AM
After that I tryed to connect 8 devices but right now the BLE Stack full does not support more than 6 master connection. The error i retreived calling the connect function is the same 0x41 that i was retreiving disconnecting and reconnecting.
So I think that the previous problem is a bug of the stack: if you have 6 connection (the maximum) and a connection disconnects and the user core send another connection request the stack thinks that it is full of connection and does not accept it.
2020-06-11 12:06 AM
After that I tryed to connect 8 devices but right now the BLE Stack full does not support more than 6 master connection. The error i retreived calling the connect function is the same 0x41 that i was retreiving disconnecting and reconnecting.
So I think that the previous problem is a bug of the stack: if you have 6 connection (the maximum) and a connection disconnects and the user core send another connection request the stack thinks that it is full of connection and does not accept it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.