NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello. I'm currently working with the STM32WB55 controller and the Nucleo demo board. I successfully used the BLE heartrate example. Now, I try to tailor the example for my needs because at the end I would like to run a similar application on the STM...
Dear Members,Is there any STM32 product spesifically for ANT+ ?Examples ? Dev board ?Thanks
Hi All,I am quite new to LoRa so if I am in the wrong forum area I do apologise. If anyone has any information based on my issues below I would appreciate a reply.I have followed the setup guide from STMicroelectronics for the P-Nucleo-LRWAN2:I have ...
HelloI am implementing the SBSFU on STM32WB. Thus I have a question on the figure 53 page 88 in UM2262 Rev 6.I need to have the "Loader" inside the "Active image", since the active image links the BLE software stack and OTA will be done via BLE. So t...
and i also checked the radio.send function its work properly that means spi work properly but data is not sending .please help me any one
I am trying to print the debug messages in different c files to check the flow of execution. Debug messages like;BLE_DBG_CRS_STM_MSG("RX Characteristic is added Successfully 0x%02X\n", CRSContext.CRSRXCharHdle); 2. APP_DBG_MSG("-- G...
HI, I have a custom board STMWB55CGU6. I have connected it to a ST-LINK V2 to try to debug it. I have connected the correct pins (GND, NRST, SWDIO and SWCLK) but the STLINK is unable to detect the PCB. It shows the error as shown in the picture below...
I have checked all the required positions of the jumpers on the STM32 Nucleo board as follows: • JP1 - USB STL • JP2 ON • JP3 ON I have installed Java 8. I have selected ST-Link mode, the device is visible in device manager as STLink Virtual PortI al...
Stack versions: LRWAN_V1.2.1Hardware: CMWX1ZZABZ-091 Murata moduleHello,I have some devices connected to Orange french lora network. I loose one device and looking on uplink history, i see that the last uplink show a frame counter with the value 6553...
I'm trying to port simple Keil project (which works on my custom STM32WL board) to CubeIDE and got to a point where it compiles and I can flash the board using stlink+GDB (I patched the stlink to add STM32WL support). However, it seems like when I t...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.