2020-01-06 2:54 AM
Stack versions: LRWAN_V1.2.1
Hardware: CMWX1ZZABZ-091 Murata module
Hello,
I have some devices connected to Orange french lora network. I loose one device and looking on uplink history, i see that the last uplink show a frame counter with the value 65535. I think it is a mater of counter overflow from device or network side. I update my soft to do again a lora_init() after 65000 uplink, but i think this should be handle by the lora stack?
Regards,
Fabrice.
2020-07-08 1:09 AM
Hello,
I have the same issue,I don't know if you solved the issue meanwhile ?
I see also a strange behaviour when there is an overflow, data sent to The Things Network are randomised.
Best regards,
Salvatore.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.