STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4119 Views
  • 0 replies
  • 3 kudos

How to update FUS trough OTA

Hello there !When I use Monitor RF to upgrade firmware(0x7000 offset on CPU1) and wireless stack (0xF000 offset on CPU2) trough OTA : It works.But when I want to upgrade (or just rewrite the same version of FUS) trough OTA at 0xF000 on CPU2 : it does...

DMatt.1 by Associate II
  • 1607 Views
  • 3 replies
  • 0 kudos

FUS_STATE_ERR_UNKNOWN || STM32WB50 Firmware update error

Attempting to update STM32WB50 Firmware using STM32 Cube Programmer in Boot mode (Boot0 pin connected to VDD)download stm32wb5x_FUS_fw_1_0_2 - Start Address 0x080EC000download stm32wb5x_FUS_fw - Start Address 0x080EC000download stm32wb5x_BLE_Stack_...

Aishwarya by Associate III
  • 1260 Views
  • 0 replies
  • 1 kudos

BLE stack installation

Hello.I'm using a custom PCB with the STM32WB50 controller. I think I successfully upgraded the FUS from version 0.5.3 to 1.0.2 and finally to 1.1.0 (when I read 0x20030030 I get 01010000). Then I tried to install the BLE light stack as described in ...

andreas23 by Associate II
  • 3512 Views
  • 5 replies
  • 0 kudos

Resolved! STM32WLE5JB doesnt exit from stop mode with LPTIM.

I'am using STM32WLE5JB with LOWPOWERMODE_STOP(0,1,2) to deacrease power consumption. Although I configured LPTIM with LSE for 2 sec period to wake up, device doesnt exit from stop mode. I tried LPTIM with LSI the result was same. Here is My code LPTI...

0693W000001sDrtQAE.jpg

Data reception stops at Mac_802_15_4_FFD in the sample code.

HelloThis is my first time using the community. I don't understand how to use the communityLet me ask you a question.Currently, I am checking the reception of IEEE802.15.4 on the board of STM32WB55 Nucleo Pack using the sample Mac_802_15_4_FFD.Stm32w...

MNitt.1 by Associate II
  • 3983 Views
  • 10 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.