2020-10-16 12:55 PM
I have set the TIM2 with the following code:
__HAL_RCC_TIM2_CLK_ENABLE();
htim2.Instance = TIM2;
htim2.Init.Prescaler = 0;
htim2.Init.Period = 80;
htim2.Init.RepetitionCounter = 0;
htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
HAL_TIM_PWM_Init(&htim2);
TIM_OC_InitTypeDef tim2OC1;
TIM_OC_InitTypeDef tim2OC2;
tim2OC1.OCMode = TIM_OCMODE_PWM1;
tim2OC1.Pulse = 20;
tim2OC1.OCPolarity = TIM_OCPOLARITY_HIGH;
tim2OC1.OCFastMode = TIM_OCFAST_DISABLE;
tim2OC1.OCNPolarity = TIM_OCNPOLARITY_HIGH;
HAL_TIM_PWM_ConfigChannel(&htim2, &tim2OC1, TIM_CHANNEL_1);
tim2OC2.OCMode = TIM_OCMODE_PWM1;
tim2OC2.Pulse = 40;
tim2OC2.OCPolarity = TIM_OCPOLARITY_HIGH;
tim2OC2.OCFastMode = TIM_OCFAST_DISABLE;
tim2OC2.OCNPolarity = TIM_OCNPOLARITY_HIGH;
tim2OC2.OCIdleState = TIM_OCIDLESTATE_RESET;
tim2OC2.OCNIdleState = TIM_OCNIDLESTATE_RESET;
HAL_TIM_PWM_ConfigChannel(&htim2, &tim2OC2, TIM_CHANNEL_2);
HAL_TIM_Base_Start(&htim2);
HAL_TIM_PWM_Start(&htim2, TIM_CHANNEL_1);
HAL_TIM_PWM_Start(&htim2, TIM_CHANNEL_2);
__HAL_RCC_GPIOA_CLK_ENABLE();The timer is working fine and in the debugging mode I find the value of counter increasing normally but when I connect the scope to the channel_1 pin PA_0 ==> A3 on the board no PWM out of the controller I checked with channel_2 also.
I also tried the code generated from Cube IDE mx with adding the TIM Start and PWM Start in the main but with no result.
So what's wrong ?
2020-10-16 1:20 PM
You need to initialize the pin(s) with the appropriate (TIMx) alternate function mode.
2020-10-18 1:44 AM
I'm sorry I missed to attach the code for initializing PWM pins
__HAL_RCC_GPIOA_CLK_ENABLE();
/**TIM2 GPIO Configuration
PA0 ------> TIM2_CH1
PA1 ------> TIM2_CH2
PA2 ------> TIM2_CH3
PA3 ------> TIM2_CH4
*/
GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF1_TIM2;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);And also the PWM not working is it possible that the pins are damaged ?
2020-10-18 8:14 AM
It seems like the code should work, although I'm not super familiar with the STM32WB series. It's possible the pins are damaged but way more likely there's an issue in the code.
Attach a debugger, step through the code, see if/where it's stuck, inspect the TIM registers to see if it's working, and the GPIO registers to see if they're configured correctly, etc.
2020-10-19 12:13 AM
I already did that and checked the timer registers the code doesn't stuck at any point and the CNT register is working fine and CCRx values are correct that's why I assumed that the pins may be damaged.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.