STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Using MB1389D Nucleo64 with STM32WL on top of Arduino board

Hello there,I've sucesssfully built the app AT_SLAVE app and downloaded it to my the board.When connected trough USB everything works fine.I've the enable USART1 to be able to communicate with the STM32 via D0/D1 of the arduino connector.I have no co...

LCHIV.1 by Associate
  • 1134 Views
  • 1 replies
  • 0 kudos

P-Nucleo-LRWAN2 stops working on TTN

Cross-post on The Things Network (TTN) forum: https://www.thethingsnetwork.org/forum/t/st-p-nucleo-lrwan2-stopped-working I followed the 'Getting Started' instructions:UM2587 Getting started with the P-NUCLEO-LRWAN2 and P-NUCLEO-LRWAN3 starter packs ...

0693W000007CKsFQAW.png 0693W000007CKw7QAG.png 0693W000007CKzpQAG.png

Resolved! STM32WB dual mode at the same time?

Is it possible to use MCUs in the STM32WB line in both Bluetooth LE and Bluetooth Classic modes at the same time? I've seen that it does "dual mode", but not whether it can do both at the same time.Thanks

DHoff.2 by Associate
  • 1320 Views
  • 1 replies
  • 0 kudos

Why can I not freely develop my own protocol using the STM32WB? Why restrict to only Bluetooth an 802.15.4

Why am I limited to using the Bluetooth and 802.15.4 MACs? The hardware can clearly do FSK and DSSS, so why the striction? Why are you restricting entrepreneurs from innovating and developing free and open source protocols for use in the 2.GHz space ...

Resolved! STM32Wb55 fail

When i connect the STM32WB55 with PC via USB cable on ST-Link Port, This window is prompted on my screen with Fail.TXT file showing message as shown in PIC  what can be the reason and issue?I have connected WB first time to my PC

0693W000007B1VAQA0.png 0693W000007B1V5QAK.png
KGupt.1 by Associate III
  • 1241 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.