2021-06-09 2:53 AM
Development Environment: KEIL (Free License)
보드 : DISCO-L072CZ-LRWAN1
Hello
To build a monitoring system with the LoRa protocol now.
It is being developed as a 'DISCO-L072CZ-LRWAN1' board.
I turned off the 'ST-LINK' built into the board to check the minimum current in the 'STANDBY mode' (removed SB37).
I have a 'ST-LINK V2'.
Can I connect my current 'ST-LINK' to 'DISCO-L072CZ-LRWAN1' for flashing?
I thought using the SWD interface in CN8 would be a flash.
So we connected SWD PINs of 'ST-LINK' and 'DISCO-L072CZ-LRWAN1'.
I tried to flash by connecting 'SWCLK' pin and 'SWDIO' pin on 'CN8' No.2 and No.4
However, neither 'KEIL' nor 'ST-LINK utility' recognized the board.
I would appreciate it if you could let me know if I'm taking the wrong approach.
Solved! Go to Solution.
2021-06-09 3:14 AM
You'd also need a common ground and the VTarget on the ST-LINK's pin 1 or 2 to power the buffers.
I've always used the on board ST-LINK, you might want to review the schematic thoroughly.
2021-06-09 3:14 AM
You'd also need a common ground and the VTarget on the ST-LINK's pin 1 or 2 to power the buffers.
I've always used the on board ST-LINK, you might want to review the schematic thoroughly.
2021-06-09 5:37 PM
I didn't write about the GND.
Of course, we connected the common GND.
Does 'VTarget' mean to connect the power of the board to STLINK?
Did you mean 'board ST-LINK' included in the board? If correct, I posted a question because I wanted to remove the power of the ST-LINK and connect the external ST-LINK for development.
Thank you for your answers.
2021-06-09 11:52 PM
I solved it.
As you said, I connected VTarget with 3.3v on the board.
I don't think it was recognized because it wasn't connected to 3.3v. Thank you very much for your reply.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.