NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I am using ble advertising example beacon project. I have initiated util scheduler/sequencer. I have registered inside scheduler exti buttom task that is used to standby whole device but it does not stop, device wakup imediately after standby. I am t...
In Table 150 ("STM32WLE5xx/55xx configuration in system memory boot mode") on page 380.In the section "USART2 bootloader", "USART1" must be replaced by " USART2".Thank you.JL
Hi,I have a custom PCB using the STM32WB55 running at 32MHZ. For some reason my board is drawing high current ~40mA. I’m trying to rule out anything I may have missed connection wise on the WB. Would anyone have any ideas if this high current draw is...
I have a new design based on STM32WB55CGU6 Microcontroller. I wanted to use the MLPF-WB55-1E03 IPD Device for Maching Network. However, the device seems to be out of stock world wide.Can I replace it with MLPF-WB55-02E3?
I'm new at STM32. I have a STM3255WBRGV which i want to aquire data from sensors with, then send the data with BLE. Kinda like the p2pexamle project. I have seen almost all youtube videos and googled a lot about setting up BLE, without using an examp...
My questions are as follows, based on the use of the SUBGHZ_Tx_Mode Example project for the NUCLEO-WL55JC board. (1) Can I use it to transmit LoRa radio on 868MHz? It doesn't specify in the readme file. (2) When editing the .ioc file in STM32CubeIDE,...
Hi...I am using STM32WB5MMG MCU..to optimize the power consumption I am using HAL_PWREx_EnterSTOP2Mode() to put the controller in sleep mode.. But after power cycling the board multiple times the power consumption increases and not stable always...Wh...
i am using STM32 Nucleo Pack LoRa HF band sensor and gateways. The Gateway has STM32L073RZT6 low power MCU with ST LoRaWAN_GS. I am trying to connect the LoRaWAN gateway with LORIOT network server and after following all the procedures, i.e configuri...
Hi there,We purchased STM32WB5M-DK for our project. In STM32WB5M, We have only one SAI Interface. We connected PDM Microphone (MP34DT01-M) on SAI1 A. I want to play the audio signal with speaker through speaker amplifier. I'm using TAS2770 speaker am...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.