NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I am using Serial Wire Debug (SWD) to trace some debug information while using the STM32WB55CGU6U MCU. Based on UM2609, the default maximum size of the SWV trace buffer on a PC = 2,000,000 packets. This buffer is stored in the heap of the STM32CubeID...
I'm working on a mobile project based on the STM32WB5MMG.First, we bought a P-NUCLEO-WB55 and had a look at some of the example projects.After a good experience with the Nucleo board, we decided to build HW around the controller.Now the HW is working...
The datasheet only shows the current of the STM32WB55 at 3.3V; what happens at 1.8V? In particular: how is the radio section affected by the voltage drop? Does the current drawn in TX and RX remain the same even at 1.8V? (Rx 4.5 mA / Tx at 0 dBm 5.2...
STM32Cube/Example/BLE_AT_Client/readme.html requirement:This example requires to have STM32WB5M module flashed with latest BLE_AT_Server application from STM32CubeWB package.I downloaded stm32cubewb_v1-12-0 and patch-cubewb_v1-12-1 but these zips do ...
Hello,I have an application with STM32WB55 that is working without a problem using UTIL_SEQ_Run(UTIL_SEQ_DEFAULT); and i am using app_ble_update_data function to update the packet data but i would like to start advertising without using UTIL_SEQ_Run(...
Hello! I'm trying to interface with a sensor that requires a repeated start condition.Datasheet: https://www.mouser.com/datasheet/2/348/ROHM_S_A0005047448_1-2562246.pdfI have other sensors on my I2C bus that I can communicate with. I also get '1' on ...
I have a custom board running the i cube lrwan (class A). I m going to deploy it in the field, so I dont want any messages coming on the UART. Is there a way to disable it ?When I add too many print statements for debugging, the LoRa Initialisations ...
Greetings, i have been trying to set up a STM32WLE5CC MCU to wake up from STANDBY Mode after a period of time (30 seconds for the testing phase, 1 week in the final product) using HAL Library functions.Unfortunately i have not been able to accomplish...
SUBGHZ Radio Cfg_DioIrq() describes mapping the radio interrupts to separate IRQ lines but NVIC only has one Radio IRQ interrupt.Are the radio interrupts all just muxed into that one interrupt?Does the mapping need to be applied to all IRQ lines none...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.