STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4119 Views
  • 0 replies
  • 3 kudos

STM32WL55 does not receive uart input after a certain amount of time passes after sending RF periodically

Hi I am testing with STM32WL55I programed that MCU transmitted LoRa signal periodically and transmitted data via uart1 periodically.At first, MCU can recieve data via uart1.After a certain amount of time, MCU can't transmitted some bytes via uart1 on...

0693W00000GXDEBQA5.png

MLPF-WB55-02E3 connection to STM32WB55V WLCSP_100.

I have some questions on the response here:https://community.st.com/s/global-search/MLPF-WB55-02E3?t=1636577804470The response references MLPF-WB55-01E3 but I think it should be MLPF-WB55-02E3 for the WLCSP_100 package. Can you confirm the 65 ohm im...

TEben.2 by Associate
  • 723 Views
  • 0 replies
  • 0 kudos

Resolved! Read STM32WLE5C8U6 & STM32WLE4CCU6 UID

Hi,I'm working on the two MCU's STM32WLE5C8U6 & STM32WLE4CCU6 and I need to know the UID in order to indentify each of the products.In the doc it's written that both have UID but there is no address to read them.What I'm missing ?Best regards,

ABric.2 by Associate II
  • 1840 Views
  • 2 replies
  • 0 kudos

Where can I find API PHY_802.14.5 for STM32WB?

Hi,I am using STM32WB55 to develop a PHY 802.15.4 application with custom MAC. I found only the Phy_802_15_4_Cli example, but there are ASCII like commands. Can you provide byte oriented commands for working with PHY?

AZent.1 by Associate
  • 890 Views
  • 0 replies
  • 0 kudos

Sending BLE message data via UART

I am attempting to send a file via BLE (Windows app -> STM32WB55), I've found that the ACI_GATT_ATTRIBUTE_MODIFIED_VSEVT_CODE event is called whenever a packet is received by the board however I am unable to find where the actual packet data is store...

OCatt.1 by Associate II
  • 1785 Views
  • 1 replies
  • 0 kudos

Count on Tim2 going past ARR?

I have a simple example where I take an A/D sample from a pot every 15ms. I then modify CCR1-4 on both TIM2 and TIM1 AS WELL AS ARR registers on TIM2 and TIM1. ARR is updated with a value and ALL CCRx are updated with that value - #define. I notic...

SWenn.1 by Senior III
  • 1881 Views
  • 5 replies
  • 0 kudos

STM32WB10CC antenna connection shorted to GND.

For the new STM32WB10CC chip, there is no specification on default state of the RF pin, however, it should not be shorted to GND. Hardware has been verified with high confidence that short is not due to physical issues, is software short to GND on RF...

GChan.3 by Associate
  • 801 Views
  • 0 replies
  • 0 kudos

Resolved! Ask for AN5156 Layout recommendations's origin Altium PCB file?

Hi, I recently read the AN5165——Development of RF hardware using STM32WB microcontrollers,and the page25~page27 show the STM32WB55's reference design.But I didn't find the file on the offical website.Could you please share the files named:MB1427A---U...

skycham by Associate II
  • 4682 Views
  • 9 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.