NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
The question is how do I connect the output of the pdm and how do I connect the input of the clock to the sensorThis is the sensorsThis is the mcu chip (stm32wb55cgu) Thank you for your supportefiehrman@gmail.com
Hello,I am working with a custom board with the STM32WB5MMG SoC and I am receiving a hardware error timer overrun 0x02 after some time. After that the BLE interface stops working.There is any way to prevent this error? Is related to the hardware de...
Hi,I am working with the STM32WB55 Nucleo board to create a Zigbee device being able to connect to a Philips Hue Bridge v2.1. Using a 2.4GHz sniffer with wireshark I am able to follow the communication which goes through the following steps with no p...
Hello,I'm working on a project using Zigbee as main communication network.In this project we develop two devices :One as server and coordinatorOne as client and routerWe based our hardware on STM32WB5MMG.I used the examples of Zigbee_OnOff_Client_Rou...
I have P-NUCLEO-WB55 it worked initially well with BLE stack. Later I have ported Zigbee Stack but things were not working out. I went back and loaded the BLE stack now, but it is not even advertising with p2p sever application. I have tested the GPI...
Hi All, I'm currently using an STM32WB5MMG module on two devices to establish a Zigbee connection between them.My project is based on the example called "BLE_Zigbee_Dyn"(one device should also be able t communicate using BLE ) implementing everything...
Hi all,I'm trying to develop on the Nucleo USB dongle. I'm creating an empty Zigbee project with the FW 1.12.1 I configure the minimum in cubeMX the project crash in startup_stm32wb55cgux.s I'm running FUS V1.2.0.0I'm using the wireless copro : stm3...
I'm trying to get a handle on using the Sub Ghz middleware along with the processor's low power modes. I've configured an X-NUCLEO-LPM01A to power the NUCLEO-WL55JC, following the instructions from the STM32WL webinar, so I can take some measurements...
I'm trying to use Pa7 for an external falling edge irq without success. I have pb1 and pb4 working as expected, but not Pa7. Is there anything special about using EXTI9_5_IRQn vector?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.