STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

NUCLEO-WL55JC1 join failed when connecting to The Things Network (TTN), but TTN Console accepts the join request

I am running the LoRwWAN_End_Node example on the NUCLEO-WL55JC1 I've followed the steps set out in the following video:https://www.youtube.com/watch?v=8KNfrWoa1fwI am connecting to an existing local gateway on the TTN, and not using my own gateway as...

0693W00000GZ6tQQAT.png
MMcal.11 by Associate
  • 2037 Views
  • 1 replies
  • 0 kudos

On RX Framing error, UART_DMAAbortOnError can corrupts ongoing TX transfer resulting in 65536 bytes transfered. HAL bug ?

Hi,I use STM32Cube_FW_WB_V1.12.1 on a STM32WB55, with generated init code and HAL functions.I have setup a circular DMA for RX of UART1 and use HAL_UART_Transmit() when I need to send data.I'm communicating with a device (GPS module) that can be conf...

NSAUG.1 by Associate III
  • 1288 Views
  • 0 replies
  • 1 kudos

Resolved! Low level drivers and HAL drives

I see 2 types of drivers. one are under ll , e.g., "stm32wbxx_hal_exti"and one under hal e.g., "stm32wbxx_ll_exti"Why are there two types for each?Can EXTI C2EMR2 be configured via the hal drivers and not the ll drivers?

0693W00000GYpa7QAD.png
DS.4 by Senior II
  • 2013 Views
  • 2 replies
  • 0 kudos

P-NUCLEO-LRWAN2 FW gateway Protocol Documentation

hi I was looking for protocol documentation for provided firmware for these devices,the thing is, i cant set up the gateway properly to connect to the Chirpstask server.there is some ACK requested by the server and not provided by these devices, but ...

BYusu.1 by Associate
  • 1084 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.