NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I detected a problem : If the MX GPIO_Init(); is called before the MX_APPE_Init(); the HAL_GPIO_Togglepin not work.To solve it, I call MX_GPIO_Init(); after the MX_APPE_Init();
So this is my third day working on this problem.I have created an P2P server project based after the example and the MOOC videos.It works just fine, no problem during the first 60 seconds. The current consumption is around 200uA during advertising.Bu...
I have been using the WB since it was alpha release 0.x.y and so I have a long-established proprietary app running on the STM32WB55RG Nucleo board. Using the BLE full stack, configuring the GAP role as (GapRolePeripheral | GapRoleCentral) and subsequ...
I am using P-NUCLEO-WB55.I set 3 buttons (SW1 / SW2 / SW3) to GPIO_EXTI. I confirmed that an interrupt is generated when the button is pressed.After that, if the middleware STM32_WPAN (BLE) is enabled, no interrupt will occur even if the button is p...
I am using the L462E try to connect an IoT platform. But I am not sure which communication protocol it is using? Is it using HTTP, MQTT, or CoAP??
Hi, Thanks to a previous question and the very clear answer of an ST employee. I understood the idea of the example LoRaWAN_End_Node and that it was not necessary to re-write the falling asleep but to use the one already present. (here Custom sleep a...
Not able to start project in STM32CubeMX after board selection of P-NUCLEO-WB55 RF kit.Do we require any license for this?Please provide information for the same.Thanks!
Hello, I am very interested in using the STM32WL for a wireless application. Is the matching circuit already included in the chip (so I just have to add an antenna) ? I don't find any information about this.Thanks.
Hi I'm designing a LoRaWAN end node based on RAK3172 and LoRaWAN_End_Node example. The frequency band is 868 MHz but i want to transmit on single frequency for example 868500000 Hz. I read the example but I don't know how to send packets only on sing...
I am currently trying to create a wireless sensor network using STM hardware and ZigBee.I'm new to this type of development and I'm struggling to figure out what hardware I need.I currently have a STM32F746G-DISCO MCU, I would like to use this board ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.