2021-11-27 11:01 PM
Hi
I'm designing a LoRaWAN end node based on RAK3172 and LoRaWAN_End_Node example. The frequency band is 868 MHz but i want to transmit on single frequency for example 868500000 Hz.
I read the example but I don't know how to send packets only on single frequency. How can I do that?
Thanks.
2021-11-29 1:37 AM
Welcome, @Estej.1, to the community!
LoRa not only uses a specific, given frequency for transmission, but a spread spectrum method. Maybe it would be helpful to have a look at the information from e.g. Wikipedia: LoRa/LoRaWAN or Chirp Spread Spectrum.
Regards
/Peter
2021-11-29 5:55 PM
Are you sure you want LoRaWAN and not LoRaP2P ?
Perhaps grep the source for "_REGION" and sources under Middleware/LoRaWAN/Mac/Region
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.