NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I'm working with the STM32wb55ceu MCU which states that it has 512K of flash memory starting from address 0x08000000.However, I realized that if I compile and run the follow program, it will hard fault when attempting to read the value from flash (li...
Trying to port code written for WB55 or WB50 onto a WB15. Obviously there's less memory available, but apparently zero documentation on what this means in the Real World. I've managed to squeeze a version of my basic application into the WB15 by maki...
Good Day, I got myself a pair of LoRa-E5 mini which has STM32WLE5JC single-core. I would like to program them in a way in which they would communicate by using a channel and address id to each other. kindly give me a refernce to how to program them i...
We designed a customized board based on STM32WLE5JB SoC without the 32k LSE crystal to save cost. However the Sub-GHz radio doesn't work - LL_RCC_HSE_IsReady() always returns 0 and no radio interrupts generated. Is it because the LSE not being solder...
Hello everyone,We are currently trying to experiment with the STM32WB5M for it to be integrated in our project as a radio co-processor module.We have ported nimble stack (https://github.com/apache/mynewt-nimble) on our application MCU to act as an ho...
hello , i'm following this tutorial LoRaWAN with STM32 Getting Started: Part 1, LoRaWAN with STM32WL Overview - YouTubeand i want to know why targeting STM32WL as end-node instead of STM32LO and How I can buy this material decomposer not a complete...
I have a customer that wants to update the wireless stack on their custom assy. This has been implemented successfully following the procedure set detailed in AN5185. Please note that this is not an OTA upgrade and the stack is upgraded via applica...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.