2022-02-16 9:16 AM
Hello everyone,
We are currently trying to experiment with the STM32WB5M for it to be integrated in our project as a radio co-processor module.
We have ported nimble stack (https://github.com/apache/mynewt-nimble) on our application MCU to act as an host stack using HCI over UART. The port has been validated with a nrf53 has a controller.
We are now trying to experiment using the STM32WB5M in "Transparent Mode" with HCI over UART (we are using the STM32WB5M development kit with LPUART1 as transport).
We end up in a situation where we are able to correctly advertise, connect to the radio (the CONNECTION_COMPLETE event is send by the STM32WB and received by the host stack and applicative layer). But the connection drops after ~3seconds, and the STM32WB doesn't send any event to notify the host stack).
The issue can be replicated using the unmodified "BLE_TransparentMode" project from cubeMX on the STM32WB5M development kit. And connect it to the STM32CubeMonitor-RF application.
The following "Scripts" to be played by STM32CubeMonitor will replicated the behavior we are experiencing :
# Script recording starts on 16/02/2022 11:40:05
Send(HCI_RESET)
Send(HCI_READ_LOCAL_VERSION_INFORMATION)
Send(HCI_READ_LOCAL_SUPPORTED_FEATURES)
Send(HCI_SET_EVENT_MASK;0x2000800002008090)
Send(HCI_LE_SET_EVENT_MASK;0x00000000000FFE7F)
Send(HCI_LE_READ_BUFFER_SIZE)
Send(HCI_READ_LOCAL_SUPPORTED_FEATURES)
Send(HCI_READ_BD_ADDR)
Send(HCI_LE_SET_ADDRESS_RESOLUTION_ENABLE;0x00)
Send(HCI_LE_CLEAR_RESOLVING_LIST)
Send(HCI_LE_SET_ADDRESS_RESOLUTION_ENABLE;0x01)
Send(HCI_LE_SET_ADVERTISE_ENABLE;0x00)
Send(HCI_LE_RAND)
Send(HCI_LE_SET_RANDOM_ADDRESS;0xDEE0005E586D)
Send(HCI_LE_SET_ADVERTISING_DATA;0x03;0x20003B0000000000635F7465675F6D65735F6C706E5F656C62203D20060102)
Send(HCI_LE_SET_SCAN_RESPONSE_DATA;0x08;0x20003B0000000000635F7465675F6D65735F6C706E5F657477656E794D0907)
Send(HCI_LE_SET_ADVERTISING_PARAMETERS;0x0030;0x0060;0x00;0x01;0x00;0x000000000000;0x07;0x00)
Send(HCI_LE_SET_ADVERTISE_ENABLE;0x01)
# Script recording ends on 16/02/2022 11:49:34
The STM32WB will advertise with the name "MYNEWT" and the connection will be dropped a few second after being established without the host stack being notified.
With the same configuration with an nrf52/nrf53, the connection is done and we are able to discover services and exchange data.
Do you have ideas on why the STM32WB has this behavior ?
Thank you,
Regards,
Romain
2022-02-21 7:13 AM
Hello,
Indeed, if any services are discovered by the STM32WB, it will disconnect few second after the connection. In your script, there is no service created, so a disconnection occurs. You should at least initialize GATT layer with the following command:
Send(ACI_GATT_INIT)
Best Regards
2022-02-25 12:53 AM
Hello Remy,
Thank you for your answer,
Is this a STM32WB special requirement ? I haven't seen in the Bluetooth SIG specification the fact that no services present should lead to a disconnection.
Regards,
Romain
2022-02-28 5:28 AM
Hello,
No, it's inside smartphone application, if no services are discovered, the smartphone operate a disconnection.
Best Regards.
Remy
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.