NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
The readme.txt file for BLE_HeartRate_ota contains the following:@note This application is not supported by CubeMx but has been copied from the project BLE_HeartRate generated by CubeMx with some modifications in order to be able to download it...
While debugging an application on the M0+ core of a STM32WL55JC device, the debugger showed what appears the incorrect execution of an ARM machine instruction.The codesnippet at the beginning of the execution is shown in Image #1:(the original C cod...
Good day,On a brand new SMT32WB5MMG MCU, I have found that the One-Time Programmable area is not empty. See the image. The OTP area starts at 0x1FFF7000. There is also some data right before the OTP area - what is that doing there as well?For context...
I am using STM32WB55, and try to implement power saving functionality.I am using FreeRTOS and have a task that checks for the sleep conditions, and if they are met, it shall put the device in the lowest power mode possible. Wake-up is then triggered ...
Im' following this tutorial of STM32WB55: https://www.youtube.com/watch?v=CKYWy7LKL68&list=PLnMKNibPkDnG9JRe2fbOOpVpWY7E4WbJ-&index=19&ab_channel=STMicroelectronicsAll is fine until I try to generate code. It gets stuck at the moment of "Copying libr...
Hi, from the micropython repository there is a note on a problem regarding address resolution, it is reported at this link.Are there any details about it? is this a known and solved problem? or still open?Thanks and regards
The quartz used for HSE on the nulceo-wl55jc and on the reference design for stm32wl is NX2016SA 32MHz EXS00A-CS06465, which has a 10pF load capacitance (the BOM for reference design even mentions 8pF, but the quartz reference is actually 10pF).The m...
Hi everyone,I modified the project https://github.com/STMicroelectronics/STM32CubeWL/tree/main/Projects/NUCLEO-WL55JC/Applications/LoRaWAN/LoRaWAN_End_Node so that my MCU - STM32wle5c8 can communicate with lora but I get the error ("IRQ_CRC_ERROR") a...
I have function to receive Dev EUI, APP Key, and NWK Key data from UART. Then, I want to put and replace of Dev EUI, APP Key, and NWK Key in se-identity.h with my own data which I have saved in flash memory. But, an error occurs when only include my ...
Hi everyone,I'm trying to convert our IoT Sigfox sensor from EFM32 to STM32 architecture.As a beguinner on STM32, I'm using an LSM100A eval board based on STM32WLE5CC.Can anybody explain me how to create a simple Sigfox project ? I just want to send ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.