STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4119 Views
  • 0 replies
  • 3 kudos

How to pass data between two cores (STM32WB55)

Hi,I have a program running on the M4 core of the STM32WB55 and would like to pass a data buffer to the M0 for transmission over BLE (notification). I'm having a really hard time understanding how to pass the data between the cores and was hoping for...

kcire L. by Associate III
  • 923 Views
  • 1 replies
  • 0 kudos

STM32WB Client Mode

Hi, I want to application with STM32WB55 mcus. One mcu will be a server with the hrstm application, and the other mcu will be a client and listen to the data and print listening data with uart to the screen. But I couldn't find any sample code as cli...

0693W00000HqAzTQAV.png 0693W00000HqB2eQAF.png 0693W00000HqB3IQAV.png
MErkc.1 by Associate II
  • 1220 Views
  • 1 replies
  • 0 kudos

Lora Ping Pong example with specific address

Hi, I'm trying to adapt ST LORA poing pong example to my own need. To do thaht I'd like to update the code to use specific address for master and slave. For example I'd like to set in source code the address 12000 to master and addresse 13000 to slav...

SBaro.11 by Associate III
  • 831 Views
  • 0 replies
  • 0 kudos

Resolved! How to change APP_TX_DUTYCYCLE from remote?

I want to change the tx-duty cycle when my application is running (from a scheduled downlink for example), I guess i just could replace the define with my own variable, but that would be overwritten as it is outside the user code sections. What is th...

ABläs.1 by Associate II
  • 1805 Views
  • 2 replies
  • 1 kudos

Uplink issues after ChirpStack registration

HelloI'm using the NUCLEO-L073RZ board and the I-NUCLEO-LRWAN1 shield. I am trying to register with ChirpStack, but there is a problem.After connecting power, I can check JoinRequest and JoinAccept messages from ChirpStack Application Server.However,...

HJung.5 by Associate
  • 938 Views
  • 1 replies
  • 0 kudos

Resolved! STM32CubeMonitor-RF DLL or CLI

Hi everyone,I am trying to create a windows pc app to talk to the STM32WB board using the dongle.I want to run some scripts, e.g., write to characteristic, connect, read an etc.I saw that STM32CubeMonitor-RF can already run scripts via some text file...

DS.4 by Senior II
  • 1214 Views
  • 1 replies
  • 0 kudos

nucleol073rz's App_eui keeps changing to 0

I'm using nucleo l073rz and I'm trying to connect to Chirpstack.But it doesn't have an uplink. When I checked the JoinRequestMessage, all contents of App_eui were zero. I set it to the original App_eui using the serial port, but it returned to zero i...

0693W00000LwF1OQAV.png
sjung.11 by Associate
  • 1450 Views
  • 2 replies
  • 0 kudos

STM32WL55 MX_IPCC_Init() error from config tool.

On STM32WL55, i have made a skeleton for an app including subghz in fsk, with mx config tool. When building i get an error on one core and warning on the other about MX_IPCC_Init(),wich is declared static in main.c and used in main so i can thing the...

Xynium by Associate III
  • 1774 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.