2022-01-24 2:38 AM
On STM32WL55, i have made a skeleton for an app including subghz in fsk, with mx config tool. When building i get an error on one core and warning on the other about MX_IPCC_Init(),
wich is declared static in main.c and used in main so i can thing the init is done.
from ipcc_if.c :
void IPCC_IF_Init(void (*IPCC_IF_CommandRcv_cb)(uint32_t channelIdx),
void (*IPCC_IF_AcknowledgeRcv_cb)(uint32_t channelIdx))
{
/* USER CODE BEGIN IPCC_IF_Init_1 */
/* USER CODE END IPCC_IF_Init_1 */
/*Initialise the ipcc, initialises MSP*/
MX_IPCC_Init(); <- ERROR undeclared
/* Enable C2AHB3 peripherals clock. */
LL_C2_AHB3_GRP1_EnableClock(LL_C2_AHB3_GRP1_PERIPH_IPCC);
/* IPCC EXTI (AIEC) line fo
Regards
JP Lathuile
2022-01-24 3:01 AM
Hi
Got a solution.
In the config tool
in project manager/advanced setting uncheck static witch is checked by default
Regards
JP
2022-03-30 6:11 PM
Looks like a bug in the templates that should be taken care of by ST. I replaced that call with the following code, copypasted from the main() template and got ipcc_if.c compiling.
IPCC_HandleTypeDef hipcc;
hipcc.Instance = IPCC;
if (HAL_IPCC_Init(&hipcc) != HAL_OK)
{
Error_Handler();
}Not yet sure if it behaves correctly yet. I can see that HAL_IPCC_Init() (defined in Drivers/STM32WLxx_HAL_Driver/stm32wlxx_hal_ipcc.c) will reset number of CPU registers.
#if defined(CORE_CM0PLUS)
IPCC_CommonTypeDef *currentInstance = IPCC_C2;
#else
IPCC_CommonTypeDef *currentInstance = IPCC_C1;
#endif
if (hipcc->State == HAL_IPCC_STATE_RESET)
{
/* Init the low level hardware : CLOCK, NVIC */
HAL_IPCC_MspInit(hipcc);
}
/* Reset all registers of the current cpu to default state */
IPCC_Reset_Register(currentInstance);
/* Activate the interrupts */
currentInstance->CR |= (IPCC_CR_RXOIE | IPCC_CR_TXFIE);
/* Clear callback pointers */
IPCC_SetDefaultCallbacks(hipcc);
/* Reset all callback notification request */
hipcc->callbackRequest = 0;
hipcc->State = HAL_IPCC_STATE_READY;
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.