NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Dear ST Support Team,I am using STM32WB55 with firmware stm32wb5x_BLE_Thread_dynamic_fw.bin release V1.23 and application based on samples in STM32CubeFW. I flashed two devices and set both devices:OT_LinkMode.mRxOnWhenIdle = 1U;OT_LinkMode.mDeviceTy...
HiI have 6 BLE peripherals with some ADC's. I need to make sure that all 6 devices sample at the same time. The Accurracy needs to be below 500 micro seconds. Is there a way to synchronise devices via BLE stack ?Thx
Dear community, On my board, a STM32WB55CEU6. My aim is to add the DFU BLE possibility for code update.On the first picture, you will see mu CUbeProgrammer Interface.After click on "Read FUS infos", i'm able to read status.The FUS is ok, but the stac...
Hi All,I'm currently using an STM32WB5MMG on my project and I'm struggling to reach the expected power consumption.Please note one known error on the PCB: the RF_OUT and ANT_IN pins, which should be connected to GND according to the datasheet/guideli...
i am using LoRaWAN_End_Node_FreeRTOS in STM32WL55JCIX in that for send the data i used APP_TX_DUTYCYCLE and set 43200000(12 hours) for send data to gateway there is delay getting of 20 to 25 minutes every data send is there any solution for that ???
We are currently developing two LoRaWAN-based products using STM32WL55J (battery powered and Mains AC). Both devices are designed to sample sensor data every 30 seconds and transmit it according to a defined daily duty cycle.However, we are facing ch...
Hello everyone,I’m working on a project using the STM32WB55RG microcontroller with FreeRTOS, and I’m trying to put the MCU into STOP Mode 2. The system is supposed to wake up regularly using the RTC.I’m using LL libraries to configure the power regis...
Dear ST members,I'm designing a new board with STM32WBA65RGV6 in LDO power supply scheme. The datasheet and reference manuals are not clear how to connect certain pins in this configuration. Please, clarify the queries below:Is VDDSMPS to be connecte...
Hi,I'm trying to make continuous TX CW signal on 868.1 MHz or 432.4 MHz with the nucleo stm32 WL55jc2 without success. I spend a lot of times but sometimes goes wrong.I'm looking for somebody who as experienced with SUBGHZ and ping-pong as my app is ...
Hello ST team,We are using the STM32WL5MOC6HTR module, which does not include the STSAFE-A110 secure element.However, in the STM32WL5MOC6HS variant, the PB8 pin is used to power the STSAFE chip (VDD_STSAFE).In our setup (with the HTR module), when we...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.