STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Resolved! RF switch supply from GPIO pin as output?

Can anyone confirm if it is okay to supply the RF switch directly from a general purpose output of the STM32WL? This way I could control when the switch is working or when the antenna is isolated (off) from the circuit.I see in the datasheet for the ...

AZube.2 by Associate III
  • 2813 Views
  • 2 replies
  • 0 kudos

Resolved! Can I use SMPS in microcontroller for AC-DC converter?

The STM32WB55 microcontroller have SMPS internally.   Can I use it to convert AC power to DC power for the microcontroller?   If possible, I want to supply RF inductive charging power directly to the microcontroller.  

KKIM.6 by Senior II
  • 3116 Views
  • 6 replies
  • 0 kudos

Resolved! Missing command ACI_HAL_TONE_START in BLE full stack 1.13.3

Hello,From 1.13.0 to 1.13.3, the command ACI_HAL_TONE_START was removed (get Unknown command return). The release note indicates that some HCI commands were removed not ACI commands.Is it an error or should we prepare to move to the full extended sta...

AnthonyS by Associate II
  • 2697 Views
  • 5 replies
  • 0 kudos

[STM32WLE5CC] Firmware behavior according to power

Currently, we are using the STM32WLE5CC MCU.Some MCUs do not operate normally when the same firmware is inserted into several MCUs. (Abnormal current, delays in Uart log output, RF is not transmitted)If a higher voltage (4.4V) than the MAX operating ...

BHwan.2 by Associate
  • 1529 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.