2022-10-20 11:09 AM
2022-10-28 8:29 AM
Hello @Community member ,
I suggest you to try with the very simple examples under "Projects\NUCLEO-WL55JC\Examples\PWR" to verify your consumption. Like that you won't use the radio part that may lead to an over consumption
As you have the X-Nucleo-LPM01A Board, you can use STM32CubeMonitorPower software tool which is very useful to do current measurements.
Regards
Louis
2022-10-20 3:49 PM
Some aspects are relevant also for Stop modes:
2022-10-27 7:46 AM
Hello @Community member ,
You mean STM32Cube_FW_WL_V1.2.0 ?
Which hardware are you using ?
How are you measuring this consumption ?
Regards
Louis
2022-10-27 8:50 AM
Hello Louis,
yes i mean STM32Cube_FW_WL_V1.2.0
The hardware is this one: RAK3272S Breakout Board | RAKwireless Documentation Center
The board itself has the RAK3172 at its core, integrating a STM32WLE5CC chip. It has Ultra-Low Power Consumption of 1.69 uA in sleep mode.
The low level development is descriped here: RAK3172 Module Low Level Development Reference | RAKwireless Documentation Center
I measuring the consumtion with the X-Nucleo-LPM01A Board and a digital multimeter.
Greetings
E_T
2022-10-28 8:29 AM
Hello @Community member ,
I suggest you to try with the very simple examples under "Projects\NUCLEO-WL55JC\Examples\PWR" to verify your consumption. Like that you won't use the radio part that may lead to an over consumption
As you have the X-Nucleo-LPM01A Board, you can use STM32CubeMonitorPower software tool which is very useful to do current measurements.
Regards
Louis
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.