2022-11-14 1:40 AM
Hello,
I am currently using STM32WB55 with QSPI external flash.
Currently, the plan is to use it without Bluetooth, for now.
I am able to write and read the flash in the program.
The plan:
The question:
Best regards,
A.S.
Solved! Go to Solution.
2022-11-23 1:13 AM
2022-11-23 1:13 AM
2022-12-14 10:25 AM
>>Is there a better way of doing this?
Probably, what are your metrics?
QSPI NOR Flash is very SLOW, both writing and usual 4K block erasure.
QSPI NAND Flash is unvarnished, so you're likely to have to deal with correction, deblocking, and wear leveling. The erase blocks sizes are perhaps unmanageable for most MCU, so you'd need more complex file systems.
eMMC is a better/faster route, the BGA's might be unmanageable for some
XTX has some perhaps easier to integrate designs. XTSD01G/XTSD02G/XTSD04/XTSD08G
2022-12-14 11:42 AM
We use QSPI Flash because it consumes less power than the other options.
By "better way", I mean is there a standard/example of using embedded memory for a similar case (data logging)?
Most examples show either transmitting sensor data via wireless/wifi or using an sd card where they use a card reader to transfer the data. In this case, I am able to save the sensor data into the flash, but I am unsure how to move the data to the PC for analysis. I am looking for a data logging example in which the data could be transferred to a PC without desoldering the flash chip.
Currently, we are using QSPI NAND from Alliance Memory (AS5F38G04SND-08LIN).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.