STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Resolved! Do I need a new RF CERTIFICATION of the STM32WB5MMG on a custom pcb with body distance LESS than 20cm?

In the datasheet of the STM32WB5MMG Module is writtenThe module antenna must be installed to meet the RF exposure compliance separation distance of “20 cm�? and any additional testing and authorization processes as required.in the sections FCC and IS...

BGeig.3 by Associate II
  • 1413 Views
  • 1 replies
  • 1 kudos

BLE stack questions regarding connection and advertising

I have some question related to the BLE stack code. Specifically regarding GAP operation.My device is the peripheral.On first connection to my device from peer :How long can a 'connection procedure' take. From when the stack is receiving a connection...

DS.4 by Senior II
  • 1109 Views
  • 1 replies
  • 0 kudos

Problem LoRaWAN EU868 certification in Ukraine

Hi everybody,I have to problem with LoRaWan EU868 certify in Ukraine, specifically as follows:I am using ABZ module as CMWX1ZZABZ-091 to develop product, and I set ABZ module such as:+ firmware based on source code en.i-cube lrwan v1.3.0+ used Lora m...

npham.1 by Associate
  • 1889 Views
  • 1 replies
  • 0 kudos

SHCI_C2_BLE_Init Fails

I'm trying to start up CPU2 on an STM32WB55. I've looked at various examples and I seem to be doing all the right things. SHCI_C2_BLE_Init returns 0xFF in payload[0] which corresponds to SHCI_FUS_CMD_NOT_SUPPORTEDI have FUS V1.2.0.0 installed and the...

TWood.4 by Associate III
  • 1229 Views
  • 1 replies
  • 0 kudos

Resolved! Programming and Running BLE stack in CPU2

Greetings,Currently the project has a requirement for a Custom BLE server profile. I have a few doubts, for which I'm seeking clarifications.I flashed the 'stm32wb5x_BLE_Stack_full_fw' v1.14 at the specified memory location as per the release notes. ...

ABN by Associate III
  • 2534 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.