2022-12-23 5:21 AM
What is the meaning of the time data in last 4 columns in table 3 ("Stop 2 versus Standby gain, function of Tx interval time") and 4 ("Stop 1 versus Stop 2 gain, function of Tx interval time") of AN5568? What is the meaning of different percentages (1%, 5%, 10%, 20%)?
Thank you very much!
2023-01-04 5:48 AM
Hello @CSale.1 and welcome to the community !
Theses tables give you the consumption gain in % when you change from one low power mode to another.
The values in the 1%, 5%, 10% and 20% columns represent the periodicity of the Tx.
For example, if I take the first line of table 3 ie a High Power 22dBm emission of 1.48 seconds repeated every :
- 37 minutes in STOP2 gives a power saving of 1% if we switch the low power mode to STANDBY
- 13h 15 minutes in STOP2 gives a power saving of 20% if you switch the low power mode to STANDBY
This show that if you switch to a power mode with a lower consumption, you will have a big difference if you do not transmit too often.
Then to summarize those two tables, you can see there is a bigger difference of consumption between stop1 and stop2 than between stop2 and standby.
I hope I helped you
Regards
Louis
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.