NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
HiI have a strange problem with my p-nucleo board(MB1355C)Using the example as reference DFU_Standalone (STM32Cube_FW_WB_V1.12.0\Projects\P-NUCLEO-WB55.Nucleo\Applications\USB_Device\DFU_Standalone)I am able to jump to bootloader and perform DFU upda...
please help check the schematic of stm32wl55ccu7 and try to solve the heating issue and abnormal condition.
Hi team, I am trying to load the program in to the STM32WBRG MCU using ST-LINK/V2-ISOL we are able to succeed the loading and verified the test code using the internal 16MHz RC oscillator, but while using the External 32MHz
Hello, i got two STM32 Nucleo-WL55JC2 (dual core) and i want to create a radio communication between these two MCUs. I've downloaded the STM32WL Package and i want to upload the pingpong dual core example on my two cards. (I'm using CubeMX 6.7.0 and ...
I followed the STM32WB Getting Started Series: Part 9 on topic of updating FW to a newer version and reviewed relevant App Notes and HTML from the repository. I use ST-LINK to STM32WB55 Nucleo eval board with STM32CubeProgrammer 2.12.0. The demo code...
I have a previously working app and both examples _EndNode and AT_SLAVE.The board worked well for about 30 hours.I could not get the other 2 examples for this board to compile and work.After a change, neither app joins the network reliably. The gatew...
The sampling frequency is 256kHz, it is an ADC that collects ECG signals.(The question is really not about ADC), what should I belong to with this question?My problem is that the analog signal is output in four channels in parallel after the ADC, whe...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.