2023-01-06 5:10 AM
I am using the STM32WB55CCU6 low energy Bluetooth microcontroller. As I am not using the USART interface and don't need to support a Real Time Calendar clock, I didn't attach an external low frequency crystal resonator. However, I am wondering whether this was a mistake as the BLE Bluetooth interface requires a low frequency clock [ RTC ] and it doesn't seem possible to use the internal low frequency clock [ LSI ] - disabling RTC also disables the RF section in the .ioc file.
Is there some form of work-around that allows for the use of the internal low frequency oscillator ?
@JBlac.1
2023-01-11 1:55 AM
Hello,
If you don't have an external low frequency crystal resonator, you should use HSE/1024 clock as input for RF system wakeup clock. The BLE doesn't require RTC to work, RTC is required in the application for the timer for example.
Best Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.