STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Resolved! Running Nucleo WB55 off a 3.7V LiPo battery

Nucleo-WB55RGThe docs mention that it can be run off a button cell & also mention that the 3V3 pin can be used to power the board. Is it possible to run the board off a 3.7V LiPo battery? My application is pulling 7ms & using BLE 

Help - Problem with BLE_AT_CLIENT on B-U585-IOT02A

Hello everyone,I am currently working with the BLE_AT_CLIENT example on the B-U585-IOT02A and have previously updated the integrated STM32WB5M according to the instructions in readme.md (Wireless Coprocessor Update). The example's start screen appear...

Delta1 by Associate II
  • 407 Views
  • 0 replies
  • 0 kudos

Utility Sequencer not starting task

Apologies for cross post, I couldn't find a way to delete the other post or how to change which board to post it to.I'm trying to set up the Utility Sequencer to run an acquisition task followed by an signal processing task, see code snippets below.W...

Design for STM32WL55CC + 22dbm, 868MHz

Hello,I am currently designing a custom PCB with the STM32WLE5CC (QFN package) targeting +22 dBm in the 868 MHz frequency band.I have been following the reference design based on the MB1720 board, which is specifically described as being for +22 dBm ...

blnc___0-1763975427911.png
blnc__ by Associate II
  • 525 Views
  • 0 replies
  • 0 kudos

Resolved! LORA-E5-HF(stm32wle5jc)

Respected Sir/ Madam,    AS i'm using LORA-E5(stm32wle5jc) module communicating point to point Radio Frequency and AT Command also. We are config SubGHz for Radio Send and Receive Functions in Loop Mode . No Response received from this.  By using AT ...

SYAMALA by Associate II
  • 3673 Views
  • 6 replies
  • 0 kudos

STM32WLE5JCI6 with LoRa-E5 Development Kit.

Hi techs, I have a problem with the LoRa configuration with the LoRa-E5 Development Kit. How to do the Pin configuration for the LoRa point to point communication. I have tried multiple ways to do but the communication is not happening, and I also tr...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.