STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

STM32WLE5 code error??

I am trying to use the following well written example to have two boards communicate using GFSK:sub-GHz FWMy code compiles error free up to the Example Application section. If I then replace my main with the GFSK main on github. I get the following...

0693W00000aIrVlQAK.jpg
SWenn.1 by Senior III
  • 704 Views
  • 0 replies
  • 0 kudos

VREF+ pin on P-NUCLEO-WB55 board

Hi, on P-NUCLEO-WB55 board, the VREF+ pin is connected to VDDA which is the analog power supply. See the picture.My understanding is that this pin is an output when the internal VREF (2.048V or 2.50V) is used. Does this connection mean the use of int...

0693W00000aIbmCQAS.jpg
WQ by Associate III
  • 2057 Views
  • 3 replies
  • 0 kudos

Resolved! STM32 program only read data from sensor once and then freezes

The given example on LoRaWAN_End_Node software pack is transmit temperature, humidity, and pressure data. My main objective is to do the same thing but instead of send those three datas, I want to send the parsed GNSS data like how the SimOsGetPos di...

0693W00000aIihJQAS.png
Wtuya.1 by Associate
  • 2561 Views
  • 1 replies
  • 0 kudos

STM32 and sx1262MB2CAS Shield

Hello thereI am completely new in STM32, I need to use two SX1262MB2CAS shield to tx with one of them and rx from the other one.Do you know which drivers i will need and how to configure the stm32cubeide project to have acces to two stm32?

AMitj.1 by Associate
  • 1459 Views
  • 1 replies
  • 1 kudos

A Hint to Drive the VL53L4CD using STM32WL55JC

Hello, I tested the VL53L4CD with the Nucleo-STM32F401 using the ST-Example and I got Ranging readings. However, when I port the code to use the STM32WL55JC, I always get an I/O Error.I use the same pin configurations to drive the sensor as in the Ex...

0693W00000aIb4ZQAS.png 0693W00000aIazVQAS.png
AElgh by Associate III
  • 1380 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.