NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Case 1: without STOP2 mode UTIL_SEQ_SetTask or HW_TS_Start working fine.Case 2: without UTIL_SEQ_SetTask or HW_TS_Start calling, the device can go to sleep and wake up without any problem.case 3: when the device wakes up and after the device wakeup,...
1. Issue: When connecting a PC to a device for the first time, disconnecting the connection after turning off the device's power, and then turning on the device's power, the PC and device should automatically reconnect, but they are not connecting.Pr...
Hi I am trying to play a little bit with STM32WLE5 MCU in order to receive raw wM-Bus packages (mode S, T and C). But I need help in setting up the radio part. Is there anyone who can provide a piece of code on how to setup the radio communication fo...
Hi, I'm trying to send data via LoRa with two Nucleo wl55 boards, one receiving, and one sending. I made the code from the SubGHz_Phy_PingPong example, and altered only the process where the "ping-pong" happens. I'm trying to debug both boards, but t...
Hello,The STM32WB55 on our custom board doesn't ever go into stop2 mode. Our application needs to activate BLE and advertise for a fixed time at startup, so that the system can be configured and started. After this period BLE is no longer needed, so ...
Hello, I wanted to ask if anyone actually is doing (or has already done successfully) the STM32WB Getting Started Series on youtube (STM32WB Getting Started Series - YouTube) and the according Nucleo Pack (P-NUCLEO-WB55 - Bluetooth 5 and 802.15.4 Nuc...
Hello!!I developed a BLE product with STM32WB55CEU. I am preparing certification.To be certified, the STM32WB55CEU must be set up for RF testing.I set it up with Transparentmode FW for P-nuleoboard. But it didn't work.Different chipset seems to be th...
I am following this tutorial for setting up my STM32WB55 dev kit. When I generate the code and try to compile I get the following error:../STM32_WPAN/App/custom_stm.c:22:10: fatal error: common_blesvc.h: No such file or directory../STM32_WPAN/App/cus...
Hello Community,I am making a custom requirement with LoRa using STM32WLE5CCxx. The parameters for the P2P communication are given below:Frequency: 868MHzSpreading Factor: 7Coding Rate: 4/3Bandwidth: 125KHzPreamble Length: 8 TX Power: 14dBm Another t...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.