2023-04-18 10:34 PM
Hello Community,
I am making a custom requirement with LoRa using STM32WLE5CCxx. The parameters for the P2P communication are given below:
Frequency: 868MHz
Spreading Factor: 7
Coding Rate: 4/3
Bandwidth: 125KHz
Preamble Length: 8
TX Power: 14dBm
Another thing to add I am using the RFO_HP pin transmitter section.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.