NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I have developed a program on the NUCLEO-WB55RG which contains a STM32WB55RGV6 MCU. Sadly our small company dont have the necessary equipment for RF design so we are planning to use the STM32WB5MMG module, which contains STM32WB55VGY MCU and all the ...
Hi,I'm using STM32CubeIDE 1.4.0 to build an application (BLE Hid) for the P-Nucleo-WB55 board. It's looking for an include file stm32wb55xx.h which is missing. Any idea where to find this file?Thanks,Jim
Hello,I'm using the Nucleo-WL55CJ kit to test the Lora connectivity with TTN server.At first, all worked fine and I received my data, but now the kit is unable to join the networt with the following error "DevNonce is too small".Any idea?Thanks.
I have generated code with Lorawan. I am reading data from HTU31D sensor, the sensor pushes the same data (first stored data) in lorawan. Thank you
Before I recommend the STM32WB55 for our project, I'd like to know if what we want to do is even possible. Our application requires ultra-low power and so I'd like to limit the use of the micro where ever I can. We have a Gray code encoder that we ne...
Hi,how can I use the Temperature Measurement Cluster with Zigbee? I have configured STM32 CubeMX with an endpoint and the cluster, but "zcl.temp.meas.h" doesn´t contain functions for handling the cluster. Only "ZbZclTempMeasClientAlloc" and "ZbZclTem...
The example project shown below builds and downloads successfully and halts at main(). The ST-LINK appears to connect and start successfully. It is when I click on run that the ST-LINK server says "Target is not responding, retrying..."I changed abso...
Hi everyone!I need to have several pins acting as ADCs to get data from different analog sensors connected at the same time. In board's datasheet I see that this board has 1 ADC with multiple channels (12 channels to be precise).The problem is that C...
Hi,This is my architecture:1 board client.5 board servers.In the client i have:A routine that try to connect, pair and update MTU size of all the servers.A routine that send and receive message from the paired servers.Right now i have some problem be...
I am evaluating the ASTRA1B demonstration board. I powered up the board, with factory firmware, via USB and attached an STLINK-V3MINIE debugger/programmer to the J300/STDC14 connector on the expansion board to a PC running TT.Output to console worked...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.