NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello,I would like to know the capacity of external memories supported by STM32 MCUs wireless family :- STM32WBA- STM32WB- STM32WB0- STM32WL I looked up in the datasheet of all referencies but I didn't find the information. Thank you for your help. B...
hi allI'm working on a P-NucleoSTM32WB boardI've try BLE_p2pServer_Ext exemple with CM0 loaded with stack_full_extended.bin and it works wellon the other hand I've a simple Custom app that works wellafter tweaking .ld file for getting it to work with...
I’m using a STM32WB5MMGHx module on a battery powered device. I need to put the module in Stop mode 2 in order to have a better battery life. After reset when the module enters the stop mode for the first time it stops advertising as it should. After...
Created a new project for the STM32WB55CE microcontroller and I am trying to configure the SPI1 using the Pinout & Configuration tool. However, SPI1 is greyed out with the message "I2S1 must be disabled". I tried looking for the I2S1 and I think it i...
Hello! I am using STM32WB as a MCU for a custom pcb. I am using the BLE Sensor firmware but slightly altered for our application. The question I have is - If I want to perform data acquisition intermittently (let's say every 5 mins) and transmit dat...
AN5669 seems to indicate that the BLE Object Transfer Service is available on STM32WB devices. Are there any technical documents or examples showing how this would be used in an STM32Cube application?
Hello i am looking for specifications for the antennas supplied with the p-nucleo-lrwan packages. Unfortunately i cannot find any specific information about the supplied antennas such as impedance, gain, etc in the documentation of the products. I wo...
Hello, I am using 2 NUCLEO-WBA52CG dev boards with project STM32Cube_FW_WBA_V1.1.1\Projects\NUCLEO-WBA52CG\Applications\BLE\BLE_p2pServer. I am using IAR 9.40.1 My pc wireless is Intel® Wi-Fi 6 AX200, pc is running win10 pro (latest) While getting th...
I followed the instructions posted here to enter the bootloader and successfully connect to the MCU via USB using STM32CubeProgrammer. When I attempt to load code the following error occurs: 09:12:45 : USB speed : Full Speed (12MBit/s) 09:12:45 ...
Hello Sir,I am working on STM32WB. I am using the reference of STM32WB Dongle. The reference Dongle design used STM32WB55CGU6U MCU Part Number. I used STM32WB55CGU6 ( Without 'U') MCU Part. Bluetooth is not working with my PCB.is there any Difference...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.