2024-01-09 5:23 AM
Hello,
I'm currently working with an STM32 microcontroller, and I'm facing a challenge related to the internal Real-Time Clock (RTC). Specifically, whenever I attempt to set the date and time using the internal RTC, my system crashes. I've reviewed the code and checked for potential issues, but I haven't been able to identify the root cause. Has anyone in the STM32 community encountered a similar problem when configuring the internal RTC? If so, could you share any insights, potential reasons for this behavior, or troubleshooting steps that might help me resolve this issue? Your assistance would be greatly appreciated as I work to address this problem in my project.
Here my Set date and time function,
"
/**
* @fn ErrorStatus RTC_SetTimeAndDate(void)
* @brief Function to use Set date and time into Internal RTC
*
* @return SUCCESS / ERROR
*/
ErrorStatus RTC_SetTimeAndDate(void)
{
RTC_TimeTypeDef sTime;
RTC_DateTypeDef sDate;
if(HAL_RTCEx_BKUPRead(&hrtc, RTC_BKP_DR1) != 0x32F2)
{
/** Set the Time and Date **/
sTime.Hours = AppControl.mRTC.mTime.mHours; // BUILD_HOUR;
sTime.Minutes = AppControl.mRTC.mTime.mMinutes; // BUILD_MIN;
sTime.Seconds = AppControl.mRTC.mTime.mSeconds; // BUILD_SEC;
sTime.SubSeconds = 0; // (AppControl.mRTC.mTime.m100thSeconds * 10); // BUILD_SEC;
sTime.TimeFormat = RTC_HOURFORMAT_24;
sTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE;
sTime.StoreOperation = RTC_STOREOPERATION_RESET;
if (HAL_RTC_SetTime(&hrtc, &sTime, RTC_FORMAT_BIN) != HAL_OK)
{
return ERROR;
}
sDate.WeekDay = AppControl.mRTC.mDate.mWeekDays; // RTC_GetCurrentDayOfWeek(BUILD_DAY, BUILD_MONTH, BUILD_YEAR);
sDate.Month = AppControl.mRTC.mDate.mMonths; // BUILD_MONTH;
sDate.Date = AppControl.mRTC.mDate.mDays; // BUILD_DAY;
sDate.Year = (AppControl.mRTC.mDate.mYears - 2000); // (BUILD_YEAR - 2000);
if (HAL_RTC_SetDate(&hrtc, &sDate, RTC_FORMAT_BIN) != HAL_OK)
{
return ERROR;
}
}
HAL_RTCEx_BKUPWrite(&hrtc, RTC_BKP_DR1, 0x32F2); // backup register
return SUCCESS;
}
"
Thank you in advance.
Solved! Go to Solution.
2024-02-02 11:30 PM
Using internal RTC for setting date and time is not possible. If you want to create a calendar, you should use a SW solution.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-02-02 9:32 AM
Hello @Mr._Nileshkumar_Solanki
The internal RTC on the LoRaWAN context is used only for LoRaWAN and it can't be used for date and time.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-02-02 10:06 PM
Thank you @STTwo-32 for your reply,
What if I want to use internal RTC in my application.
Any another way for set date and time.
2024-02-02 11:30 PM
Using internal RTC for setting date and time is not possible. If you want to create a calendar, you should use a SW solution.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.