STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Can't detect bluetooth from B-U585I-IOT02A board

I do everything as decribled here:-stm32u5 program with  ble at client  code-on stm32wb I update fus, stack and program  BLE_AT_Server_reference.hex from STM32Cube_FW_WB_V1.17.0When i try run app @teraterm i see:Start of the STM32WB5M module AT examp...

Dziubasku by Associate II
  • 6524 Views
  • 10 replies
  • 0 kudos

Resolved! Using RadioIsChannelFree() function for multiple devices responses

Hi all,I have a setup where many devices need to to respond to a message on 868MHz from a sender. At the moment I am using random delay to space the responses but I will like to use the RadioIsChannelFree() function.Do anyone use this function? Is it...

ola by Associate III
  • 1549 Views
  • 2 replies
  • 0 kudos

Resolved! Looking for gateway compatible with B-L072Z.

Hello community,Currently, I have Lorawan gateway: p-nucleo-LRWAN1 and Lorawan node: B-L072Z LRWAN1.I'm looking forward to suggestions from you, which company gateway and node will be better than this current gateway and node. with current devices, I...

Yuvi by Senior
  • 5174 Views
  • 14 replies
  • 5 kudos

Resolved! STM32WB15 cannot connect stlink v2

I encounter the following error when connecting STM32WB15 to ST-Link V2.Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authenticationonly VDD,GND, and SWIO and SWCLK pins connected..p...

Erdincca by Associate II
  • 3224 Views
  • 6 replies
  • 2 kudos

STM32WB55 Nucleo unable to change data rate

Hello,I have been getting into BLE applications with the stm32wb55 nucleo development board. I am currently developing my application over the BLE p2pServer app. I have modified the program such that the P2PS_Send_notification() method keeps sending ...

BLE Receiving Data

Hello everybody, I am currently building a STM32 BLE software and in this software I got a very long custom loop. My problem is I want to continously check whether there is data received with BLE, if there is, process the data, and return to main loo...

Yusuf by Associate III
  • 2176 Views
  • 3 replies
  • 0 kudos

STM32WB5MM BLE Idle status

Hi, I'm developing a BLE P2P application to exchange data. I have encountered a problem while debugging. The status for the BLE when turn on is APP_BLE_FAST_ADV, but when I restart the debug sessions the status is APP_BLE_IDLE. It looks like the CPU2...

Pablo1610 by Associate II
  • 1298 Views
  • 1 replies
  • 0 kudos

STM32WB55CEU6 BLE not working

Hello,We are using STM32WB55CEU6 in one of our project and we are facing the issue in BLE. We checked all the powers and soldering related things, everything looks fine. But BLE is not able to advertise.Also, from the firmware side the same code is w...

Nishantt by Associate II
  • 3906 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.