2024-02-12 10:59 PM
Hi all,
I have a setup where many devices need to to respond to a message on 868MHz from a sender. At the moment I am using random delay to space the responses but I will like to use the RadioIsChannelFree() function.
Do anyone use this function? Is it a recommended way for avoiding transmission collision and if so are there good example on how to properly utilize this function?
Ola
Solved! Go to Solution.
2024-02-13 5:07 AM
Hello @ola
For the best coordination between multi-sender and a receiver, you need to give a small delay for each sender. For example sender one send at t=0 then sender two send after 10s, ...
So you can easily identify the sender and ensure coordination.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-02-13 5:07 AM
Hello @ola
For the best coordination between multi-sender and a receiver, you need to give a small delay for each sender. For example sender one send at t=0 then sender two send after 10s, ...
So you can easily identify the sender and ensure coordination.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-02-13 5:12 AM
Hello STTwo-32,
Cool thank you for your response. I am currently doing what you are suggesting at the moment. I use your Radio.Random() function from your subghz_phy_app.c to get a random value at startup and use this number to space the transmit responses.
That's fine. I was only checking to see if there was a more sophisticated way that I was not aware of.
Regards
Ola
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.