2024-03-11 8:52 AM - edited 2024-03-12 2:35 PM
I have one of P-Nucleo-WB55 and recently bought one more P-Nucleo-WB55 board.
We are using this board to program the STM32WB55VG6YTR microcontroller in our custom board and we have succeeded more than 20 times in programming that microcontroller using ST-LINK in P-Nucleo-WB55.
However, recently we couldn't access either our microcontroller in the custom board or the dummy microcontroller in P-Nucleo-WB55 anymore. In addition, we never succeed in using the new P-Nucleo-WB55 board.
After several trials, we found that the wire length of SWCLK was the reason.
Right now, we only can access the dummy microcontroller in P-Nucleo-WB55 using a jumper pin to connect SWCLK. If we use a normal wire (resistance < 1 ohm), we cannot access even the dummy microcontroller.
This problem is big because we have to program the microcontroller in our custom circuit board.
Does anybody have a similar problem and find a solution?
Solved! Go to Solution.
2024-03-11 9:00 AM
@KKIM.6 wrote:we found that the wire length of SWCLK was the reason.
What made you conclude that it was the length of the wire, specifically?
What length are you using?
@KKIM.6 wrote:This problem is big because we have to program the microcontroller in our custom circuit board.
Obtain a standalone programmer?
eg,
https://www.st.com/en/development-tools/st-link-v2.html
https://www.st.com/en/development-tools/stlink-v3minie.html
etc
@KKIM.6 wrote:dummy microcontroller in P-Neucleo-WB55
I guess this is probably just lost in translation, but the microcontroller on the board is fully functional - it's not a "dummy".
2024-03-11 9:00 AM
@KKIM.6 wrote:we found that the wire length of SWCLK was the reason.
What made you conclude that it was the length of the wire, specifically?
What length are you using?
@KKIM.6 wrote:This problem is big because we have to program the microcontroller in our custom circuit board.
Obtain a standalone programmer?
eg,
https://www.st.com/en/development-tools/st-link-v2.html
https://www.st.com/en/development-tools/stlink-v3minie.html
etc
@KKIM.6 wrote:dummy microcontroller in P-Neucleo-WB55
I guess this is probably just lost in translation, but the microcontroller on the board is fully functional - it's not a "dummy".
2024-03-11 9:07 AM
We can access the dummy microcontroller using a very short jumper pin connecter.
If we replace the jumper pin connecter to a normal 2.54 wire (length < 15 cm, resistance < 1 ohm), we cannot connect to the dummy microcontroller even.
This problem has happened recently with an old P-Neucleo-WB55 board.
The new P-Neucleo-WB55 board has had this problem from the beginning.
Such a problem wasn't last year.
Is there any update on the CubeProgrammer or any noticeable change?
2024-03-11 9:34 AM
Try adding more ground wires between the boards. Different Slew behaviour of different chip runs by result in excessive ground bounce
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.